Stormwater Management for Home Depot Parking in Flushing, NY
Case study: subsurface stormwater management system
A new home improvement store required a cost-saving underground stormwater management system alternate to the originally designed concrete precast system. The engineer desired a shallow underground stormwater system that could be installed under the future parking lot.
The goal was to provide a cost-effective shallow subsurface stormwater management system, with high void space, that can meet HS-25 loading requirements.
Solution and installation: R-Tank UD
The original underground stormwater system design for this project called for a large field of concrete leaching galleys. After reviewing initial pricing from contractors, the project team decided to revisit the design plans and evaluate other potential systems that would be more cost-effective and work better within the shallow cover conditions.
R-Tank UD modules were chosen to replace the concrete leaching galleys. They would reduce the total depth of the system while maintaining the load-bearing capacity for heavy traffic loads commonly found in parking lots—and provide savings to the owner.
We were involved during the redesign process and provided preassembled modules and on-site assistance during the installation. Prior to the tanks being installed, the area was excavated and regraded. A smooth base layer of stone was then added and leveled to provide a suitable base to put the tanks on.
The R-Tank modules were placed on a woven monofilament geotextile, which was placed over the level stone base. Inspection ports were added and horizontal pipe connections were made while the tanks were being placed. The system was then sealed with woven monofilament geotextile.
Once the system was sealed, a 12-inch stone layer was added to encase the system, followed by a layer of biaxial geogrid prior to pavement installation over the top.
Results
Both the engineer and contractor were thrilled with the rapid installation of the system. The R-Tank UD offered cost savings and installation efficiencies on this tight site both in section and available space.
To learn more about our capabilities and solutions, visit ferguson.com/waterworks.