Hampton Roads Sanitation District Plant Decommissioning and Line Replacement
Case Study
The Hampton Roads Sanitation District is one of the largest wastewater treatment organizations on the East Coast, managing wastewater from the North Carolina line to Virginia’s Northern Neck region. A plant decommissioning required a flow redirect and replacement of 9,000 feet of 24-inch sewer force main that had been in place since the 1950s. To meet the minimum requirements for the new use, the sanitation district needed 7,000 feet of 42-inch ductile iron and 2,000 feet of 48-inch high density polyethylene pipe.
The project was complicated by two factors. First, the line ran down the middle of Virginia Beach Boulevard, a heavily traveled and often-congested six-lane road. Second, the line was flanked by a sensitive wetlands area. The installation necessitated five tunnels underground and submergence in salt water.
The tunnels are “either under bodies of water or underneath roads carrying the public,” explained Frankie Bridgeman, president of Bridgeman Civil. “From day one, the only thing that was concerning to me was getting all the pits and the microtunnels done and tested.”
Ferguson recommendations and installation
When Bridgeman became the project’s senior manager, he turned to Ferguson, a trusted partner with a strong success record. He said the company assisted in multiple ways. It provided:
Careful project management:
Completing a project of this scale and in a complicated location required strong project planning and execution. Ferguson will “read the spec, and if something doesn’t look right there, they’ll email the owner to ask questions and to make corrections,” Bridgeman said. “Ferguson was able to work with the ductile supplier and move stuff around on the schedule.”
Expert consultation:
The original project was designed with mechanical joint fittings where the pipe came out of the end of the tunnel: An HDPE MJ adapter to an MJ 90 that rose vertically 30 feet, to another MJ fitting to reach at least a 12-foot elevation. This took place at the job site.
“What happens if one of those fittings ever leaks down the road due to stretching, age or whatever?” Bridgeman wondered. “When you’re deeper than that, who knows years from now how much it could cost you to get back down to that fitting.”
Ferguson Industrial suggested transitioning over to fully fused HDPE to avoid a deeply buried mechanical connection and possible leakage.
Environmental sensitivity:
To safeguard the surrounding wetlands and creeks, the engineers relied on a bentonite fluid — an environmentally friendly silica clay — to carry the soil back to the boring machine.
“No fish, no anything, were impacted,” Bridgeman said.
Advanced technology:
Using electrofusion to couple the riser to the pipe allowed the team to minimize the amount of equipment it used, said Rob Naquin, a Ferguson Waterworks outside sales representative.
“When you have a pit that’s 65 feet, every foot bigger is more liability, more money. Just more problems, more de-watering and all that,” Naquin said.
Because the crew didn’t need heavy machinery in the tunnel or pit, potential impacts to the environment and traffic flow were reduced, liability and costs were lowered, and potential associated problems and dewatering were averted. The 48-inch electrofusion couplings were fabricated at one of Ferguson’s ISO-certified facilities and brought on site.
“Ferguson is really the only one that specializes in HDPE, as well as the ductile and the valves and everything combined,” Bridgeman said. “Other vendors can sell you the HDPE, but they’re not fabricators. And their guy can be on a truck and here tomorrow. That did make it attractive for me to work with Ferguson.”
Additionally, Bridgeman had all his fusion techs trained by Ferguson to make sure his team was up to speed on this state-of-the-art technology. Ferguson data logged every component to provide testing reporting on the integrity of the process and verify that all the welds were done following associated ASTM standards.
Final installation: concrete, steel casing, HDPE and tunnels
The final installation consisted of eight pits — 45 feet long, 20 feet wide and 45 feet deep — and two tunnels. After pouring a concrete slab, the team installed a 60-inch diameter steel casing 46 foot deep from one side of the London Bridge Creek to the other, and ran the HDPE through the tunnels with spacers to align them in the center.
“When you have a pit that’s 65 feet, every foot bigger is more liability, more money. Just more
problems,
more de-watering and all that.”
— Rob Naquin, sales representative Ferguson Waterworks
The Ferguson advantage
“The HRSD project is a good example of our ability to work with what the customer has from a vision perspective, turn that into a drawing, offer insight from the years of experience that we have, and make it a reality.”
“The biggest value that Ferguson Industrial, Ferguson Waterworks brings to any contractor or consulting engineer is that we are a master at all different disciplines. Whether it’s ductile iron or PVC or HDPE or valves, valve automation — anything that may touch their project, we have the expertise and a group behind them. Like the HPDE Ferguson Industrial fabrication facility, which has years and years of experience to provide customers a total solution.”
“This particular project had some unique challenges. It was ductile iron in some areas and HDPE in other areas. How do you bring those two together? Where do you bring those two together? What’s the right solution?”
“There are a lot of solutions that are out there that maybe need to be vetted, as you’re going through your particular situation in understanding what exactly you’re trying to accomplish. What we — Ferguson Industrial, Ferguson Waterworks, Ferguson Enterprises — bring is a breadth of products and breadth of expertise to determine the right solution.”
— Joe Morgan, business development manager Ferguson Industrial
The results
The project was originally estimated to take two years, but it was completed in just six months. Wastewater has successfully been redirected away from the decommissioned plant, and the Virginia sanitation district’s new HDPE pipes should last, undisturbed, for years.
“It’s just a better pipeline now that won’t break and have massive sewage spills. It’s a bulletproof system,” said Naquin, who sees more projects like this one on the horizon. To update dated systems and to address rising sea levels, “there’s a lot more complicated work like this coming out,” Naquin said. “Everything’s moving that way.”
Working with a trusted partner was critical, Bridgeman said.
“Having done hundreds of projects with Ferguson and buying hundreds and hundreds of thousands of feet of HDPE from them, I was very confident going into this,” Bridgeman said. Working with Ferguson also lessened the time table.
“The fact that Ferguson was able to supply every piece of the project as a manufacturer, as a distributor. To get me every piece of this project from one person instead of having to deal with 10, it always adds to the value of the project.”
“It’s just a better pipeline now that won’t break and have massive sewage spills. It’s a bulletproof
system.”
— Rob Naquin, sales representative Ferguson Waterworks
For more information, visit ferguson.com/waterworks.