Replacement of Failed Stormwater Storage System in Harrison, NY

 

 

Case study: urgent replacement of cracked system

The top slab of an existing underground concrete stormwater storage system was severely cracked and failing. The cracked system was located underneath an existing office complex parking lot, creating potentially hazardous conditions for those who parked there. Failing concrete systems also provide ideal conditions for sinkholes to develop.

 

The solution required a stormwater storage system that would:

 

  • Fit the existing footprint
  • Be cost-friendly
  • Minimize disturbance
  • Replicate the existing system’s volume

 

 

Solution and installation: R-Tank HD

When the client realized the system was failing, they contacted ACF/Ferguson Waterworks to assist in a new design. It was determined that a replacement system using R-Tank HD could be constructed inside the existing system’s footprint by keeping the concrete perimeter intact.

 

This minimized the amount of stone required around the perimeter of the system and simplified placement and compaction of the side stone. It also saved the client time and money by reducing labor and material costs.

 

R-Tank HD Pent 7-foot modules were selected to replace the existing system due to the high void space and cover parameters. To allow for the passage of water from the tanks to the perimeter stone, the system was wrapped in SR-18 microgrid.

 

Additionally, TrashGuards were placed in the upstream drains feeding into the system to collect sediment, trash and debris.

 

 

Results

This urgent replacement was an unexpected cost for the client but was necessary to avoid compromising the safety of those parking in this lot. The replacement stormwater storage system not only fit the old system’s footprint, but also provided a budget-conscious solution to the client’s initial concern. The parking lot is safe and secure once again.

 

Visit ferguson.com/waterworks to learn more about our capabilities and innovative solutions.