Bad TXV symptoms, diagnostics, & replacement guide
The thermostatic expansion valve or thermal expansion valve (TXV or TEV) is one of the most critical, yet frequently misdiagnosed, components in modern HVAC and refrigeration systems. Responsible for precisely metering liquid refrigerant into the evaporator coil, a properly functioning TXV ensures the system operates efficiently by maintaining a constant superheat. However, when performance drops, the TXV is often the first component blamed.
For professional HVAC contractors, accurately diagnosing a thermal expansion valve saves valuable time and prevents unnecessary part replacements.
How does a TXV work?
Before diving into complex diagnostics, it is crucial to understand the three primary forces that control a TXV:
- Bulb pressure (Opening force): The sensing bulb is strapped to the suction line and contains a refrigerant charge. As the suction line warms up, the gas inside the bulb expands, pushing down on the valve diaphragm to open it and feed more refrigerant.
- Evaporator pressure (Closing force): The internal or external equalizer routes the actual evaporator pressure back to the underside of the diaphragm, pushing it closed.
- Spring pressure (Closing force): An internal superheat spring provides a baseline closing force.
When the system is running at a steady state, the opening force equals the combined closing forces. When these forces become unbalanced due to mechanical failure or external system issues, the symptoms of a bad thermal expansion valve will begin to appear.
Identifying bad TXV symptoms
Recognizing faulty TXV valve symptoms early can prevent catastrophic compressor failure. However, a failing valve often mimics other system issues like an undercharge or a liquid line restriction. True signs of a bad TXV valve include:
- Inconsistent or poor cooling: The system fails to reach the set temperature despite running continuously.
- Extreme superheat values: Superheat that is exceptionally high (over 25°F) or dangerously low (near 0°F).
- Frosting on the evaporator coil or valve: Frost forming immediately after the TXV or covering the evaporator coil indicates that the valve is restricting flow severely, dropping the saturation temperature below freezing.
- Abnormal pressure readings: Extremely low suction pressure coupled with normal or slightly high head pressure.
- Compressor issues: Low compressor amp draw due to the compressor pumping mostly vapor, or a noisy compressor if liquid refrigerant is flooding back.
Always rule out poor airflow, a dirty coil, or an undercharged system before condemning the valve, as these common culprits often present the exact same symptoms.
Using superheat and subcooling measurements for TXV troubleshooting
The most definitive way to evaluate a TXV is by measuring both superheat and subcooling. You cannot accurately diagnose a TXV by looking at system pressures alone; temperature is required.
- Measure subcooling first: Take the temperature of the liquid line before the TXV and subtract it from the saturation temperature of the high-side pressure. If subcooling is normal or high (e.g., 15–25°F) but suction pressure is low, you know the TXV is receiving a full column of liquid refrigerant but failing to feed it into the evaporator. If subcooling is near zero, your system is undercharged, and the TXV is simply starved of liquid—the valve is not the problem.
- Measure superheat: Take the temperature of the suction line near the sensing bulb and subtract the saturation temperature of the low-side pressure. The TXV's entire job is to maintain target superheat (usually between 8°F and 14°F).
- Analyze the split: If you have high subcooling and high superheat, the valve is stuck closed or restricted. If you have normal subcooling and zero superheat, the valve is stuck open and flooding the system.
Identifying TXV hunting, starving, and flooding issues
| Condition | Description | System symptoms | Superheat | Subcooling |
|---|---|---|---|---|
| Starving (Stuck closed) | The valve is underfeeding refrigerant to the evaporator. | Frost on the coil, low suction pressure, low compressor amps, warm suction line. | Very High (25°F+) | Normal to High (liquid backs up in condenser) |
| Flooding (Stuck open) | The valve is overfeeding, allowing liquid refrigerant to pass through the evaporator. | Sweating or frosting on the compressor, noisy compressor operation, high suction pressure. | Very Low (0-5°F) | Normal to Low |
| Hunting | The valve fluctuates rapidly between starving and flooding. | Extreme cyclic swings in suction pressure and suction line temperature. | Fluctuating wildly | Normal (usually) |
Hunting is often caused by an oversized valve for the system load, or poor contact between the sensing bulb and the suction line. Starving is commonly caused by a plugged inlet screen, wax buildup, or a valve that has lost its powerhead charge. Flooding usually occurs when the internal seat is damaged or debris holds the valve port open.
TXV bulb testing
If you suspect the valve is not responding properly, a hot and cold water test is the most reliable way to check the integrity of the sensing bulb's charge without removing the valve from the system.
- Prepare your setup: Attach your calibrated manifold gauges to the system while it is operating.
- Unmount the bulb: Carefully cut the insulation and unstrap the sensing bulb from the suction line.
- The cold water test: Submerge the sensing bulb entirely into a cup of crushed ice and water (32°F). You should immediately see the suction pressure drop rapidly as the valve closes. The superheat will spike. If the pressure does not drop, the valve is stuck open or the powerhead has lost its charge.
- The hot water test: Remove the bulb from the ice and submerge it in warm water (around 100°F). You should see the suction pressure rise quickly as the valve opens wide to feed more refrigerant.
- Evaluate: If the valve responds appropriately to both temperature extremes, the TXV's mechanical operation is fine. The issue likely lies in poor bulb placement, missing insulation, or an external system restriction.
TXV adjustment vs. replacement
A common question among technicians is whether a misbehaving valve should be adjusted or completely replaced. Modern TXVs rarely need adjusting unless you are fine-tuning a refrigeration system or attempting to correct a valve that another technician previously tampered with.
TXV valve adjustment
While some TXVs are adjustable, not all of them are. Often, the TXVs installed at the factory on residential equipment are non-adjustable. Before attempting any modifications, visually inspect the valve to determine its type:
- Adjustable TXVs feature a brass hex cap extending from the base of the valve. Removing this cap exposes the adjustment stem.
- Non-adjustable TXVs have a flat bottom and no brass cap.
If you have an adjustable TXV, you can change the superheat by removing the brass cap and turning the adjustment stem:
- To increase superheat: Turn the stem clockwise, compressing the spring.
- To decrease superheat: Turn the stem counterclockwise, relaxing the spring.
Important rules for adjustment:
- Never adjust a valve to fix a severely restricted or stuck valve. Adjustments are only for minor superheat corrections (e.g., dialing a 16°F superheat down to 12°F).
- Only turn the stem one-half to one-quarter turn at a time.
- Allow the system to run and stabilize for at least 15 to 30 minutes before taking new superheat readings and making further adjustments.
TXV valve replacement
If the TXV has failed the bulb test, is severely restricted by internal sludge, or has internal mechanical damage, replacement is the only option.
- Always use a wet rag or heat-blocking paste when brazing the new valve in place to prevent destroying the internal diaphragm with the torch heat.
- Ensure the new sensing bulb is securely strapped to the suction line (at the 10 o'clock or 2 o'clock position for smaller lines, or 4 o'clock or 8 o'clock for lines 7/8" and larger) and heavily insulated.
When to choose a TXV valve adjustment vs. A full replacement
| Adjust the TXV when: | Replace the TXV when: |
|---|---|
| The system is brand new, has an exceptionally long line set, and needs minor superheat tuning to reach manufacturer specifications. | The suction pressure remains completely static during the ice water and hot water bulb tests, indicating a dead powerhead or seized internal pin. |
| The valve passes the hot/cold water bulb test perfectly, but the steady-state superheat is slightly out of range. | The superheat is well over 25°F, and opening the adjustment stem counterclockwise does nothing to increase suction pressure or lower the temperature. |
| You are servicing a commercial refrigeration unit where load conditions require a specific, dialed-in superheat. | The equalizer line is frosted, which indicates internal leakage bypassing the diaphragm. |
| The system suffered a severe compressor burnout, and the valve is likely clogged with acidic sludge and debris. |
Diagnosing a thermal expansion valve requires patience and an understanding of the relationship between temperature and pressure. By carefully measuring subcooling to confirm a solid column of liquid, checking the superheat to evaluate valve performance, and performing the bulb test, you can confidently differentiate between a bad TXV and a simple airflow or charge issue.
When your diagnostics point to a failed valve, you need reliable parts fast. Ferguson is your trusted partner for premium HVAC components. Shop our extensive local inventory and on ferguson.com and ensure you get the parts you need to get the system back online and keep customers comfortable.