Close up image of acetylene torch with sparks being used on piping.
Trade Talk

Acetylene torch safety guide for plumbing and HVAC work

Whether you are installing new copper piping, repairing an existing AC unit, or tackling heavy-duty commercial fabrication, knowing how to safely and effectively operate an acetylene torch is a fundamental requirement. However, the high heat and combustible nature of these gases demand strict adherence to oxy-acetylene safety procedures.

Understanding what acetylene is, how to manage acetylene torch settings, and executing an oxy-acetylene safety checklist ensures your projects are completed to code.

What is acetylene?

Acetylene is a highly flammable, colorless gas widely used in metalworking, plumbing, and HVAC industries. When mixed with oxygen, it produces one of the hottest flame temperatures of any commercially available fuel gas. This unique characteristic makes it exceptional for tasks requiring intense, localized heat. Understanding its properties is the first step in maintaining acetylene torch safety for your customers and your crew.

Acetylene applications

The versatility of an acetylene torch allows contractors to handle a wide range of jobs. From precise pipe joining to cutting through thick metals, the applications are extensive.

Welding

Welding melts the base metals of the pieces being joined, often adding a filler material to create a strong, continuous bond. Oxy-acetylene torch systems are frequently used for gas welding steel and iron because the high acetylene cutting torch temperature can easily reach the melting point of these tough materials.

Brazing

Brazing is a crucial skill for HVAC technicians and plumbers. Unlike welding, brazing does not melt the base metal. Instead, it heats the metals and melts a filler metal that is drawn into the joint via capillary action. Because brazing requires high temperatures to melt the specialized filler, an oxy-acetylene torch is the preferred tool for making leak-proof refrigerant lines and high-pressure water joints.

Soldering

Soldering is similar to brazing but occurs at lower temperatures. It is standard practice for joining domestic copper water lines. While a simple propane torch can work for smaller pipes, an air acetylene torch provides faster, more efficient heating, especially on larger diameter pipes or in colder environments.

Oxy-acetylene vs. air acetylene

When choosing equipment, contractors typically decide between oxy-acetylene vs. air acetylene setups.

  • Oxy-acetylene: This setup uses two cylinders — one for oxygen and one for acetylene. By mixing the pure oxygen with the fuel gas, you achieve an incredibly hot acetylene flame. It is ideal for welding, cutting, and brazing.

  • Air acetylene: This system uses a single acetylene cylinder and pulls in oxygen from the ambient air to fuel the flame. While not as hot as oxy-acetylene, air acetylene is highly portable, easier to set up, and provides plenty of heat for standard plumbing soldering and light brazing.

Acetylene cylinders

Safety begins long before you ignite the torch. Proper handling of acetylene cylinders is paramount, as the gas is unstable under high pressure.

Use of acetone

To safely store acetylene at high pressures, cylinders are packed with a porous filler material saturated with liquid acetone. Acetylene dissolves into the acetone, stabilizing the gas. This is why you must never exceed a withdrawal pressure of 15 PSI; drawing gas too quickly can pull liquid acetone into your hoses, ruining the equipment and creating a severe fire hazard.

Proper storage and handling

Because of their internal structure, cylinders require specific care.

  • Keep upright: Always transport, store, and use acetylene cylinders in an upright position. If a cylinder has been laid flat, stand it upright for at least as long as it was on its side before use to allow the acetone to settle.

  • Clean cylinder valves before use: Before attaching regulators, briefly "crack" the cylinder valve (open and close it quickly) to blow out any dust or debris. Stand to the side when doing this.

  • Never transfer into other storage cylinders: It is incredibly dangerous to attempt to refill or transfer acetylene between tanks. Always rely on authorized suppliers for filled cylinders.

Acetylene torch settings and safety

Knowing how to use acetylene torch equipment properly protects you and your customers. Getting the right mix of fuel and oxygen ensures a strong joint, while strict adherence to pressure limits prevents catastrophic failures.

Types of acetylene flames

Adjusting the ratio of oxygen to acetylene creates different flame profiles. You must be able to identify these by sight.

Carburizing flame uses

A carburizing, or reducing, flame has an excess of acetylene. It features a bright, feathery inner cone. This flame is lower in temperature and is sometimes used for soldering or brazing applications where you want to prevent oxidation on the base metal.

Neutral flame uses

A neutral flame has a balanced mix of oxygen and acetylene. It has a well-defined, rounded inner cone and makes a quiet hissing sound. This is the most common flame used for welding and brazing, as it does not alter the chemical composition of the metal.

Oxidizing flame uses

An oxidizing flame has an excess of oxygen. It is shorter, louder, and sharper than a neutral flame. While generally avoided in basic welding because it can oxidize the metal, it is essential when operating an oxy acetylene cutting torch, where the extra oxygen is used to blow away the molten metal.

Types of acetylene torch tips

Torch tips dictate the size and shape of the flame. Smaller tips are used for fine, detailed soldering on small-diameter pipes, while larger, multi-flame tips (often called rosebuds) are used for rapidly heating large areas or thick metals. Always ensure the tip is clean and securely fastened before operation.

Acetylene torch safety procedures

Correct acetylene torch usage is non-negotiable for job site safety.

Regulator safety and PSI

Proper pressure management is the core of oxy-acetylene torch safety.

  • Oxygen: 5–10 PSI: For standard brazing and welding, oxygen should be set within this range. Cutting operations will require higher oxygen pressures.

  • Acetylene: 5–7 PSI: This provides a stable, hot flame for most HVAC and plumbing applications.

  • Never exceed 15 PSI for acetylene: Acetylene becomes highly unstable and explosive above 15 PSI. Never set your regulator above this critical limit.

Acetylene withdrawal rule

Drawing gas too quickly can deplete the cylinder of acetone.

  • 1/10th limit per hour for intermittent use: You should not draw more than 1/10th of the cylinder's total capacity per hour.

  • 1/15th limit per hour for full withdrawal on a continuous basis: For heavy, continuous use, the draw rate should not exceed 1/15th of the capacity per hour.

Pro tip: Keep a wrench on the acetylene valve for quick shut-off ability

If your acetylene cylinder does not have a handwheel, always leave the specialized T-wrench on the valve stem while the torch is in use. In an emergency, you need to be able to shut off the gas flow instantly.

Proper opening and closing procedures

  • Opening: Open the acetylene valve slowly, and no more than one and a half turns. Open the oxygen valve fully to seal the back-seat valve and prevent high-pressure leaks.

  • Closing: Always close the torch valves first (fuel, then oxygen). Then, shut off the cylinder valves. Finally, bleed the hoses by opening the torch valves until the regulators read zero, then close the torch valves and back out the regulator adjusting screws.

  • Have flashback arrestors and check valves: Always ensure your system is equipped with check valves to prevent reverse gas flow and flashback arrestors to stop a flame from traveling down the hoses into the cylinders.

General acetylene safety

Your safety protocols must extend beyond the torch itself. Equipping your crew with the right gear and maintaining a clean workspace are just as critical as managing regulator pressures.

Essential safety gear

Ferguson offers a comprehensive selection of personal protective equipment (PPE) to keep you safe on the job.

  • Shaded glasses/welding glasses: Standard safety glasses are not enough. Oxy-acetylene eye protection requires shaded lenses (typically shade 3 to 5) to protect your retinas from the intense light and UV radiation.

  • Welding gloves: Oxy-acetylene gloves should be made of thick, flame-resistant leather to protect against heat, sparks, and slag.

  • Welding jacket: A flame-resistant jacket or leather apron protects your torso and arms from stray sparks.

  • Leather boots: Wear sturdy, closed-toe leather boots to protect your feet from dropped heavy materials and falling molten metal.

Workplace safety

Whether you are in a customer's basement or on a commercial rooftop, strict workplace safety prevents accidents.

  • Keep work area clear of rags, oil, and flammables: Pure oxygen aggressively accelerates combustion. Never allow oil or grease to come into contact with oxygen cylinders, regulators, or hoses. Ensure the area is free of combustible debris.

  • Have an ABC dry chemical fire extinguisher: Always keep a fully charged fire extinguisher within immediate reach when performing any hot work.

Acetylene torch safety checklist

  1. Inspect equipment: Check hoses, regulators, and tips for cracks, leaks, or wear.

  2. Secure cylinders: Ensure both oxygen and acetylene cylinders are upright and chained securely.

  3. Clear the area: Remove all flammables, oil, and grease from the workspace.

  4. Equip PPE: Put on oxy-acetylene gloves, shaded eye protection, and flame-resistant clothing.

  5. Open valves properly: Open the acetylene valve slowly (1.5 turns max) and leave the wrench on. Open oxygen fully.

  6. Set regulators: Set acetylene to 5–7 PSI (NEVER exceed 15 PSI). Set oxygen to the appropriate level for the tip.

  7. Purge hoses: Bleed the oxygen and acetylene hoses individually to remove mixed gases before lighting.

  8. Ignite safely: Use an approved friction striker — never use a lighter or matches.

  9. Shut down correctly: Turn off the torch fuel valve first, then oxygen. Close cylinder valves, bleed hoses, and back out regulators.

Partner with Ferguson and stay stocked up on acetylene torches, torch accessories, and essential PPE. Shop online or visit a local Ferguson counter today.