Close up image of bottom of water heater that is leaking water onto floor.
Trade Talk

Best practices for boosting water heater lifespan

As a pro, the most valuable service you can provide a water heater customer is the guarantee of a product that delivers the kind of performance and longevity that prevents the need for repair. For your customers, a water heater is an investment — and by implementing a maintenance protocol, you can extend their water heater lifespan and mitigate the risk of premature tank rupture.

How long does a water heater last?

On average, a standard water heater has a life expectancy of 8 to 15 years. However, this lifespan is not guaranteed. It is heavily influenced by water quality, usage volume, and, most importantly, maintenance frequency.

In regions with hard water, units can fail in as little as 6 years if they aren’t regularly serviced, while a well-maintained tank in a soft water environment can sometimes exceed 15 years. When you emphasize the importance of these factors, it becomes easier to show customers that spending a little on parts now is much better than paying for a brand new tank and fixing water damage later.

Tank vs. tankless: Longevity

Standard tanks can be expected to last 8 to 15 years — the constant presence of standing water makes these units more vulnerable to internal corrosion over time. Tankless water heaters, on the other hand, do not store water and have components that can often be replaced individually. Because of this, they can be expected to last 20 years or more.

Why water heaters fail

Most unexpected water heater malfunctions stem from preventable issues like sediment buildup, excessive pressure, and component fatigue. Minerals that solidify in a tank or heat exchanger create a thermal barrier that causes components to warp and eventually crack, making annual flushing or descaling essential.

Tank vs. tankless: Failure causes

TankTankless water heater
Sediment buildup creates a layer at the bottom of the tank and damages the heating elementHard water coats heat exchanger and causes it to overheat
Internal corrosion causes leakingImproper venting causes blocks and safety shutdowns
Fully corroded anode rod causes the tank to rustIgniter breakdowns cause the unit to not ignite

Signs of a failing water heater

Popping or rumbling typically indicate that built-up sediment is trapping steam at the bottom of the tank, while leaks are more urgent as they often point to loose fittings, failing T&P valves, or potentially a ruptured tank. Finally, a loss of performance — such as water taking longer to heat or running out faster than usual — often signals a failing heating element or a clogged heat exchanger. Diagnosing these issues immediately is the best way to turn a potential replacement into a manageable repair.

Sediment removal

Mineral deposits, specifically calcium and magnesium, settle at the base of a tank or coat the heat exchanger of a tankless unit. In tank models, this sediment forms a thermal barrier that forces burners to run longer, causing the tank material to fatigue. In tankless models, scale buildup reduces flow and forces the unit to work harder, eventually leading to total failure.

Tank vs. tankless: Flushing and descaling

For tank units, perform a full system flush annually. A partial drain is insufficient for removing hardened scale. A high-velocity flush is required to clear the bottom of the tank effectively. For tankless water heaters, a descaler kit is vital for a thorough flush. Because tankless units use narrow heat exchanger tubes, minerals accumulate onto the walls quickly — you can restore efficiency by using a submersible pump to circulate a descaling solution through the unit for 45–60 minutes.

Reduce hard water damage

In areas with high mineral content, install a water softener or sediment filtration system. Reducing mineral intake is the most direct way to stop scale accumulation before it starts.

Tank vs. tankless: Softener benefits

Softeners primarily prevent the popping and rumbling sounds caused by sediment buildup at the bottom of tank units, and for tankless water heaters, source control is often a warranty requirement — many manufacturers specify maximum grains of hardness, and exceeding this can lead to premature heat exchanger failure and voided coverage.

Anode rod replacement

Typical water heaters utilize a sacrificial anode rod to prevent tank corrosion. These rods — usually made of magnesium or aluminum — are designed to corrode in place of the steel tank. They generally expire within 3 to 5 years. Once the rod is depleted, the tank has no protection against rust and will develop pinhole leaks.

Powered anode rod

For customers looking for a solution they can set and forget, recommend a powered anode rod. Unlike sacrificial rods, these do not deplete over time and provide a lifetime of protection. They are also the definitive cure for sulfur odors caused by the reaction of bacteria with magnesium rods in certain water supplies.

Mixing valve

While maintaining the tank, suggest the installation of a thermostatic mixing valve. This allows the customer to store water at a higher, bacteria-killing temperature of 140°F while safely mixing it down to 120°F at the outlet. This effectively increases the unit's hot water output by up to 50% without requiring a larger tank.

Pressure and expansion management

Water expands as it is heated. In a closed system, this expansion creates significant internal pressure that stresses the tank’s welded seams and valves. Constant pressure fluctuations are a primary cause of early tank failure.

Expansion tanks

A thermal expansion tank absorbs excess volume and prevents unnecessary stress on the water heater, so verify its presence and charge by, first, isolating the water heater and bleeding the system pressure. Use a pressure gauge to check the air valve on the expansion tank. The air pressure must be calibrated to match the home’s static water pressure. These tanks absorb excess volume and prevent unnecessary stress on the water heater.

T&P valves

Test the temperature and pressure (T&P) relief valve during every inspection by manually lifting the lever to ensure the valve snaps and shuts off completely. If the valve fails to operate or leaks after testing, it is often due to mineral debris. Replace it immediately with a certified part from our inventory.

Building recurring revenue with service agreements

Framing water heater maintenance as mechanical insurance is a great way to transform a one-time service call into a recurring revenue stream. Homeowners need to understand that regular flushes and descaling are essential to prevent catastrophic tank failure or heat exchanger damage. For tankless owners, emphasize that many manufacturers require documented professional maintenance to keep the warranty valid, making an annual agreement the only way to ensure they stay compliant and protected.

By offering a specialized service agreement, you secure a predictable income and eliminate the need to bid against competitors during an emergency. This strategy shifts your role from just an emergency responder to a trusted advisor, increasing the customer's lifetime value while providing them with ultimate peace of mind.

Whether you need an anode rod or a pro-grade descaling kit — Ferguson houses an expansive suite of water heater parts and accessories to service standard and tankless units confidently. Keeping these parts on your truck is the easiest way to turn a quick inspection into a saved tank and a happy customer. Shop with Ferguson today.