A. O. Smith residential water heater installed in home.
Trade Talk

Water heater parts checklist for pros: Essentials for every truck

When servicing a water heater, a second trip isn't just an inconvenience — it can very easily cut into profits. Every hour spent driving back to replenish water heater parts is an hour of unbillable time. To ensure your first trip to your customer is the only trip, your truck must be a mobile warehouse stocked with replacement components for both electric and gas units.

Gas water heater parts: Ignition and control

For gas units, ignition and control issues are the most frequent causes of failure. In a region with hard water, you'll see mineral buildup clog pressure relief valves more frequently. Keeping a stock of ignitors is vital, as these delicate components often wear out and are necessary to get a unit running during the initial visit. Similarly, because safety sensors, such as a water heater thermocouple, are the most common reason a pilot light won't stay lit — especially in an older, standard-efficiency unit — carrying various lengths and universal adapters is a baseline requirement.

Rounding out your gas kit with standard control valves allows you to fix older units on the spot, while having manufacturer-specific flow sensors for high-efficiency tankless installation saves both your customer from an expensive tank replacement, and you from a return trip.

Electric water heater parts: Power and recovery

Electric water heater repairs are often straightforward if you have the correct power ratings on hand. First and foremost, you should always carry water heater elements — PROSELECT offers plenty that are worth a look, with some high-durability options for areas with poor water quality. You’ll also need a full set of upper and lower thermostats that include built-in safety shut-off switches.

Water heater protection: Valves and expansion tanks

Protecting the tank’s lifespan often comes down to managing pressure and safety settings. Water heater expansion tanks are essential for absorbing pressure spikes that cause tanks to burst — keeping both small and medium sizes on your truck allows you to address these hidden system threats immediately. You should also stock pressure relief valves with different probe lengths, as these safety devices frequently need replacement after they trip or become clogged with mineral buildup.

Tankless water heater replacement parts

As high-efficiency and tankless units become more common, your truck stock must evolve with specialized electronic parts. Flow sensors are critical for units that refuse to fire despite adequate water movement, while a supply of water heater filters can quickly resolve simple "no hot water" calls caused by debris. Finally, carrying service valve kits not only simplifies the current repair, but also provides an opportunity to offer maintenance services that protect the unit's long-term performance.

Your final checklist

You got the call, and now you’re ready to load your truck. Here’s a quick recap of which parts are needed for which service:

Gas water heater partsElectric water heater partsProtection partsEfficiency parts
IgnitorsHeating elementsExpansion tanksFlow sensors
ThermocouplesThermostatsPressure relief valvesFilters
Control valvesGasketsService valve kits

FAQs

Which water heater parts are replaceable?

Most external and internal components of a water heater are replaceable, provided the storage tank itself is structurally sound. For gas units, this includes the gas control valve, burner assembly, thermocouple, and ignitor. For electric units, you can easily swap out heating elements, thermostats, and high-limit switches. On all systems, components like a relief valve, anode rod, and thermal expansion tank from trusted brands like PROSELECT are designed to be replaced to extend the life of the heater.

Which water heater parts are not worth replacing?

Generally, parts are not worth replacing if the integrity of the inner tank is compromised or if the repair cost approaches the price of a new unit. If the tank is actively leaking from the base or the interior shell is too rusted, no replacement part will fix it. On units older than 10–12 years, replacing expensive components like gas control valves or electronic circuit boards is often a poor investment compared to the efficiency and warranty of a full replacement.

Can I use universal parts for all water heater repairs?

While many components like heating elements, thermostats, and thermocouples have universal versions that fit a wide range of models, high-efficiency and tankless units often require manufacturer-specific parts. Using a generic ignitor or sensor on a specialized unit can lead to error codes or unsafe operation. For the best results, verify if a universal part meets the original specifications or if a dedicated factory replacement is required.

Now that you have your list of water heater parts, shop with Ferguson to check things off the list as you load your truck. Our comprehensive stock of parts from industry titans like PROSELECT, A. O. Smith, State, Bradford White, and Rheem ensures that no matter how rare or specific the water heater, you’ll head to the job site with the exact parts required to get it running — eliminating second trips and boosting your efficiency.