A pro’s guide to dryer vent installation & maintenance
The National Fire Protection Association approximated 13,800-15,970 home fires were ignited from washer and dryer appliances each year, spanning from 2014-2018 (Ahrens, 2020). Factors contributing to ignition included: improper installation, operation, and maintenance. Furthermore, dust, fiber, and lint were often the first to ignite. Through customer education, expert dryer vent installation, and regular maintenance, HVAC professionals are uniquely positioned to reduce these risks through proper installation and maintenance.
As one of the nation’s leading HVAC distributors, Ferguson is here to help. In this dryer vent installation pro guide, we’ll cover ways to recognize poor dryer venting and its impact, proper vent installation tips, recommended dryer vent supplies and tools, and the benefits of regular maintenance.
How can you tell if a customer’s dryer vent is improperly installed?
When working at a customer's home, there are a few key indicators that may imply their dryer vent was not properly installed. During a standard inspection, you can detect malfunctioning systems and recommend corrective action to improve efficiency, and most importantly, the home’s safety. Here’s what to look for:
1. Is the dryer ventilation system using the correct material?
DIY installations often include shortcuts or non-code-compliant materials. Check for proper connectors, tape, and ducts. If you find duct tape, flexible vinyl ducts, or other insufficient materials, discuss the consequences with your customer.
2. Do you see condensation around the dryer’s ductwork or detect humidity in the laundry area?
Condensation around ductwork typically indicates restricted airflow due to lint buildup. If this is the case, then it is likely that the ventilation is not working efficiently. To reduce fire risk:
Check the vent path distance. Measure from the dryer to the termination outside. Generally, the allowable dryer vent hose length is between 25 and 35 feet. Please consult local regulations, manufacturer guidelines, and building codes to confirm.
Inspect vertical runs and sharp turns. Because it takes more effort to push air up, vertical vent paths may cause lint buildup. Similarly, sharp turns become a collection area for lint. Check these locations, remove lint, and discuss alternative vent paths with your customer.
Examine vent hose connections. With daily use, dryers often shift. Sometimes, this loosens vent hose connections or compresses flexible aluminum ducts, also known as transitional ducts. This compression causes the lint to catch and accumulate, impacting airflow. In addition, using the wrong tape or clamps may create leaks along the vent path.
Verify proper duct size. If the ductwork is too large, then the exhaust airflow is reduced. However, if it is too small, then the airflow is restricted. Recommend a quick replacement to ensure the correct fit. This will increase efficiency and prevent potential hazards.
3. Are extended dry times reported?
In most residential applications, customers who report long dry times have poor dryer venting. Fixing the issue will not only help prevent home fires but also improve overall efficiency and energy savings.
In addition to proactively inspecting dryer vent systems, it’s important to educate your customers regarding fire safety tips. Remind them to clean the lint catch between every load. This small habit, along with regular maintenance, provides a huge impact when it comes to keeping the venting system clean and reducing the potential for house fires.
What are the benefits of cleaning the lint catch?
Helps prevent dryer vent fires
Improves dry-time
Optimizes energy efficiency
Reduces maintenance frequency for venting ductwork
Reduces callbacks related to airflow issues
Dryer Vent Installation Best Practices
If your customer recognizes the inefficiency of their existing dryer vent system, or you're working with a builder who needs clarity on your installation process, use our best practices checklist below for dryer vent installation to start the conversation.
Step 1: Check in with local inspectors
To kick off the project right, contact an inspector to confirm the local dryer ventilation requirements, such as approved vent materials, installation guidelines, and max run allowances. It is also important to reference the appliance manual for specific manufacturer specifications. If working on a commercial project, review the relevant building codes.
Step 2: Plan the vent path
Most systems require dryer vent hoses to terminate outside. Finding the shortest, straightest path from the dryer to the vent cap will improve efficiency and reduce the likelihood of dryer lint buildup. When possible, avoid vertical runs (which may require booster fans) and sharp bends that impede airflow. Generally, the maximum ductwork distance from the dryer to the exterior cannot exceed 25 to 35 feet. If a 90º elbow is required, subtract 5 feet from the total to ensure proper flow.*
*These are general guidelines. Check local regulations for the exact dryer vent allowances.
Step 3: Buy dryer vent installation supplies
From foil tape to 4-inch smooth metal duct for dryer vents, Ferguson makes it easy to get the HVAC supplies you need, fast. Here are some of our most popular dryer vent installation products:
Recessed metal dryer box - flame-resistant in-wall vent kits
Pro tip: Do not use flexible vinyl ducts; they significantly increase fire risk. If necessary, use an aluminum flexible or transitional air duct to connect the dryer to the wall. Use an insulated duct in areas without climate control to prevent condensation and lint buildup. When using a flexible duct, extend it to its fullest to minimize the ridges that often catch lint.
Pro tip: Plastic dryer hoods can degrade over time. For sunny locations, opt for a metal dryer hood with a damper or dryer vent flap. This ensures both unrestricted airflow and protection from small pests, weather, and debris.
Step 4: Install the dryer vent
Since you’ve already determined the shortest, straightest path from the dryer to the exterior, it’s time to install the vent. If installing it through a finished wall, be sure to check for existing wiring, plumbing, or ductwork. If necessary, use a dryer vent transition hose from the dryer to the wall. From there, use a 4-inch smooth metal duct. Dryer duct is commonly sold in 60-inch segments. When handling, cutting, and fitting metal ducts, wear cut-resistant gloves. Use hanger straps if necessary to maintain a slight slope towards the exit.
For commercial dryer vent installation projects, do not connect all dryer units to the same duct. Doing so may cause airflow problems that reduce drying efficiency. Not to mention, it could complicate future troubleshooting.
Pro tip: Start with a pilot hole to check your placement. Generally, exterior dryer vents require a 12” clearance from the ground. A pilot hole is a way to double-check alignment before drilling a large opening in the wall with a 4” hole saw.
Step 5: Discuss the benefits of dryer vent cleaning
Once you install the dryer vent system, it is still important to conduct regular maintenance. Doing so helps:
Prevent fires
Reduce the accumulation of lint
Avoid condensation and humidity
Optimize drying and energy efficiency
How often should dryer vents be cleaned?
Several factors influence dryer maintenance recommendations, such as the dryer type, load frequency, venting length and path, and more. For example, systems utilizing vertical runs are prone to lint buildup and moisture, requiring increased dryer vent hose cleaning. By offering a recurring service plan that includes professional dryer vent cleaning, you can generate steady revenue while ensuring your customers' dryers run efficiently and prevent unnecessary fires.
Whether you require new HVAC tools, vent installation supplies, or a dryer cleaning kit, Ferguson is here to help. Find a local branch or log in to place an order online. From keeping our homes warm to preventing avoidable fires, we’re proud to support the work you do.