Side-by-side image of installed ERV and HRV systems.
Trade Talk

ERV vs. HRV: Applications, installation & maintenance

Modern construction practices prioritize airtight building envelopes to meet energy codes, reduce heating and cooling costs, and conserve energy. While this is effective for reducing utility bills, it also creates a problem: stale, trapped air. Indoor pollutants, volatile organic compounds (VOCs), off-gassing from building materials, and everyday moisture have nowhere to escape. Homeowners are increasingly educated about these indoor air quality issues and are actively looking for professional solutions.

Your customers want fresh, clean air circulating through their homes, without sacrificing energy efficiency or inflating their utility bills to get it. This is where balanced ventilation systems come in. As a professional HVAC contractor, understanding the nuances of an energy recovery ventilator compared to a heat recovery ventilator system is essential. Knowing exactly which unit to recommend, how to install it correctly, and how to pitch an ongoing service will position your business as a trusted advisor.

When to use energy recovery ventilators (ERVs)

An energy recovery ventilator (ERV) is a balanced ventilation system that transfers both sensible heat and latent heat between the incoming and outgoing air streams. Sometimes referred to as an enthalpy recovery ventilator, this system features a specialized core that allows moisture vapor to pass through along with thermal energy.

Hot, humid climates

For contractors working in hot and humid climates, an ERV ventilation system is almost always the preferred choice. During humid summer months, the ERV core strips excess moisture from the incoming outdoor air and transfers it to the outgoing exhaust air. This moisture management prevents the home's air conditioner from having to work overtime to dehumidify the incoming fresh air. By keeping the humidity outdoors, you help your customers avoid mold, mildew, and the heavy, uncomfortable feeling of damp indoor air.

Mixed climates

ERVs are also highly effective in mixed climates that experience extreme seasonal swings. While they keep humidity out during the summer, the process reverses in the winter. During dry winter months, the ERV retains indoor moisture generated by daily activities like cooking and showering, transferring it to the dry incoming outdoor air. This prevents the air inside the house from becoming uncomfortably dry, which can cause wood floors to crack and create respiratory discomfort for homeowners. If your customers live in an area where managing indoor humidity is a year-round battle, energy recovery ventilation is the right recommendation.

When to use heat recovery ventilators (HRVs)

A heat recovery ventilator (HRV) operates on a similar principle of balanced ventilation but with one key distinction: it transfers sensible heat only. The core of an HRV allows outgoing stale air to warm up the incoming cold air, but it is completely impermeable to moisture.

Cold, dry climates

HRVs are the ideal recommendation for contractors operating in cold, dry Northern climates. In these regions, tightly sealed homes often generate more internal moisture than the frigid outdoor air can absorb. If this moisture is not removed, it leads to severe window condensation, structural rot, and poor indoor air quality. An HRV effectively exhausts this excess indoor humidity to the outside while recovering the heat to warm the fresh, dry incoming air. This heat recovery ventilation process significantly reduces the load on the home's furnace or heat pump.

Hot, dry climates

Additionally, HRVs are suitable for dry and hot climates where outdoor humidity is not a concern. Because an HRV only transfers heat, it is highly effective in environments where managing incoming moisture is unnecessary. The unit will use the cooler, air-conditioned indoor air to lower the temperature of the incoming hot outdoor air, improving efficiency without the added cost of a moisture-transferring core.

HRV and ERV installation

Whether you are performing an ERV installation or an HRV installation, proper setup is critical to system performance and customer satisfaction. Both systems require careful duct design to ensure balanced airflow and quiet operation.

Contractors typically need to run dedicated exhaust ducts from moisture-prone areas, such as bathrooms, laundry rooms, and kitchens. The fresh supply air should be routed into the main living areas, like bedrooms and living rooms, or directly into the return plenum of the home's primary forced-air HVAC system. When tying into an existing return, it is crucial to interlock the ventilation system with the air handler so the blower motor distributes the fresh air evenly throughout the house.

Proper balancing is a crucial step. If the ERV or HRV ventilation system pulls in more air than it exhausts, the house becomes positively pressurized, driving moist indoor air into the building envelope. If it exhausts more than it brings in, negative pressure can draw in unconditioned outdoor air through cracks or cause dangerous backdrafting of combustion appliances. Contractors must use a manometer or anemometer to measure the airflow at the grilles or ports, adjusting the system dampers according to the energy recovery ventilator diagram provided by the manufacturer.

Addressing condensation in HRV systems

Because an HRV transfers temperature but not moisture, condensation frequently forms inside the unit's heat exchange core during cold weather. This means that every HRV requires a dedicated condensation drain line and a drain pan to prevent water damage. You must ensure the unit is mounted level and in a location that allows for proper gravity drainage. Because an ERV core transfers moisture as vapor, condensation is rarely an issue, and many models do not require a drain, offering more flexible mounting orientations.

Maintaining HRVs and ERVs

Every piece of mechanical equipment requires regular upkeep, and ventilation systems are no exception. Routine maintenance for both systems involves cleaning the exterior intake and exhaust hoods. It is common for these outdoor ports to become clogged with leaves, snow, or insect nests, which will severely restrict airflow and unbalance the system. Inside the home, the internal fans must be inspected and kept free of dust buildup to ensure efficient motor operation.

Filter replacement is the most frequent maintenance task. ERV filter replacement should be scheduled every three to six months, depending on the local air quality, pet dander, and the specific MERV rating of the filters used. The heat exchange cores also require attention. HRV cores can typically be removed and washed with mild soap and water. ERV cores, however, are often made of specialized paper or polymer materials that can be damaged by water, so they usually require vacuuming. Because HRVs produce condensation, their maintenance also requires you to regularly clean and inspect the drain pans and flush the condensate lines to prevent clogs and biological growth.

Ongoing service opportunities

For HVAC contractors, ERV maintenance and HRV servicing present excellent opportunities to establish recurring service contracts and keep your technicians busy during shoulder seasons. When you educate your customers about the necessity of regular upkeep — like cleaning drain pans, swapping filters, and clearing port debris — you position yourself as a proactive problem solver.

Customers often do not realize that neglecting these systems can compromise their expensive HVAC equipment, lead to stale odors, and negate the benefits of balanced ventilation. By offering dedicated indoor air quality maintenance checks and bi-annual service agreements, you can seamlessly upsell these services. This not only secures steady, recurring revenue for your business but also ensures your customers enjoy optimal indoor air quality year-round.

ERV vs. HRV side-by-side comparison

FeatureEnergy recovery ventilator (ERV)Heat recovery ventilator (HRV)
Transfers heatYesYes
Transfers moistureYesNo
Ideal climate applicationsHot and humid, mixed climatesCold and dry, hot and dry climates
Condensation accessoriesUsually not requiredDrain pans and tubing
Maintenance needsERV filter replacement, core vacuumingFilter replacement, core washing, drain flushing
Installation tools & suppliesAnemometers and ductingManometers and condensate pumps
Cost$$$$$

Keep your projects moving with Ferguson

By understanding the regional climate needs, specific installation requirements, and long-term maintenance opportunities associated with each system, you can confidently guide your customers toward the best indoor air quality solution.

When you’re ready to start your next project, shop Ferguson for your ERV and HRV needs or learn more in our Ideas and Learning Center.