Overhead shot of plumber installing a dishwasher in residential home.
Trade Talk

High loop vs. air gap backflow prevention for dishwashers

When installing a new dishwasher or remodeling a kitchen, preventing contaminated sink water from siphoning back into the appliance is critical. Dirty sink water, food particles, and bacteria entering a clean dishwasher basin can cause unsanitary conditions, foul odors, and potential health hazards for your customers. When a sink drain or garbage disposal becomes severely clogged, the wastewater has nowhere to go but up.

If the drainage system lacks proper backflow prevention, hydrostatic pressure forces dirty water backward through the connected hose. The two primary methods used for backflow prevention are the high loop and the air gap. Understanding high loop vs. air gap applications is essential for ensuring code compliance, maximizing drainage efficiency, and maintaining long-term customer satisfaction.

What is a high loop for a dishwasher?

A high loop is a specific routing technique for a dishwasher drain hose. Instead of running the hose horizontally or straight down from the base of the dishwasher to the garbage disposal or sink tailpiece, the installer intentionally loops the hose upward.

The hose is routed as high as possible beneath the countertop, typically right under the sink deck, and securely fastened in place before dropping back down to connect to the drain inlet. This elevation creates a steep, inverted U-shape. Gravity effectively prevents the wastewater inside the sink from flowing backward up the hose and into the clean dishwasher basin.

While a high loop dishwasher setup is very common and straightforward, it does not provide a true physical break in the plumbing line. It relies entirely on elevation and gravity. Modern dishwashers often include a built-in check valve at the discharge pump to assist in preventing backflow, but mechanical check valves can fail due to hard water scale or debris. The physical elevation of the hose remains necessary.

High loop pros

  • Installation is fast and requires minimal extra materials or specialized fittings.

  • No additional hole needs to be drilled into the countertop or the sink deck.

  • The entire drainage setup remains hidden from view inside the cabinetry, providing a cleaner aesthetic for customers.

  • Fewer physical connections mean there are fewer potential leak points over time.

High loop cons

  • It does not provide absolute, foolproof backflow prevention; if the sink floods above the highest point of the loop, back siphonage can still occur.

  • Over time, if the hose is not strapped securely, it can sag and lose its elevated peak, neutralizing the protection.

  • It is not approved by all local plumbing codes as a standalone backflow prevention method.

What is an air gap?

A dishwasher air gap is a small, cylindrical plumbing fitting that is mounted completely above the sink deck or countertop. It actively routes the wastewater from the appliance up through the fitting and then drops it down into the sink drain or garbage disposal.

By introducing a physical break into the drainage line, it guarantees that wastewater cannot possibly be siphoned back into the dishwasher. Even in the event of a severe drain blockage where the sink fills entirely with dirty water, the physical separation ensures absolute backflow protection.

Air gap code requirements

Navigating air gap code regulations is a standard part of residential plumbing. The International Plumbing Code (IPC) and the Uniform Plumbing Code (UPC) have historically mandated strict backflow prevention measures. While many jurisdictions now accept high loops if the appliance features a check valve, strict adherence to physical air gaps is still required in numerous areas.

For example, the California Plumbing Code (CPC) mandates the installation of a physical air gap fitting above the counter for all dishwasher installations to completely eliminate the risk of cross-contamination with the potable water supply. Contractors must always verify local authority having jurisdiction (AHJ) guidelines before selecting an installation method.

Typically, the air gap fitting must be installed so that its critical level is at least one inch above the flood level rim of the sink. This elevation ensures that even a completely flooded sink cannot reach the discharge point of the air gap, maintaining the integrity of the sanitary separation.

Air gap pros

  • Provides flawless, foolproof protection against backflow and cross-contamination.

  • Universally recognized as the safest method and strictly mandated in specific regional plumbing codes.

  • Serves as a visual indicator for drainage issues. If the drain line to the disposal is clogged, water will visibly discharge onto the sink deck, alerting the homeowner before severe hidden damage occurs inside the cabinets.

Air gap cons

  • Requires a dedicated hole in the sink deck or countertop, which can complicate installations on solid stone surfaces.

  • The fitting is fully visible on the counter, which some customers find visually unappealing during kitchen remodels.

  • Prone to temporary blockages from food debris, which can cause water to unexpectedly spill onto the counter during a wash cycle.

High loop vs. air gap installation

FeatureHigh loop drainageAir gap drainage
Backflow protectionReliable under normal drainage conditionsFoolproof physical break in the line
Code complianceVaries by state and local municipalityWidely accepted; mandated in specific regions
Aesthetic impactNone, completely hidden inside the cabinetVisible cylindrical fitting on the sink deck
Installation timeFast and straightforwardModerate, may require drilling a new hole
Maintenance requirementsLow maintenance, provided the hose is secureMay require occasional clearing of food debris
Cost$$$

High loop installation

For a successful and leak-free installation, both methods require professional execution. When installing a high loop, ensure the hose is securely strapped to the underside of the cabinet or the absolute highest point possible beneath the counter. A loose or poorly secured hose can sag over time, completely neutralizing the backflow protection.

Air gap installation

When installing an air gap, pay close attention to the hose sizes. The hose running from the appliance to the air gap is typically 5/8-inch, while the downward hose from the air gap to the garbage disposal is 7/8-inch. Ensure the downward hose has a continuous, unimpeded slope to prevent standing water and unpleasant odors. Because food particles from the appliance can sometimes clog the fitting, remind your customers to periodically clean the cap and remove any blockages if they notice water spitting onto the counter. Always remember to knock out the disposal plug before connecting the 7/8-inch hose — failing to do so is a common error that leads to a geyser at the sink deck.

Communicating options to your customers

During kitchen remodels, contractors frequently encounter customers who want to remove an existing air gap. Customers often request this because they prefer a seamless, clean look for their expensive new quartz or granite countertops. In these scenarios, it is your responsibility to clearly explain the underlying code requirements and the mechanical reasoning behind backflow prevention.

Take the time to educate your customers on the real risks of property damage, foul odors, or unsanitary conditions if they choose to bypass essential plumbing codes. If you operate in a region governed by strict regulations, explain that the fitting is not optional. Offering premium, low-profile finishes that match their new kitchen faucet can often help mitigate their aesthetic concerns while keeping the installation fully compliant.

Ferguson supports your plumbing business

Whether your local jurisdiction strictly requires an air gap or you are planning a standard high loop installation, Ferguson is your trusted source for high-quality air gaps, dishwasher drain hoses, and essential kitchen plumbing accessories.

Shop air gaps and other essential components today to ensure your next installation is seamless, sanitary, and up to code.