PEX-A vs. PEX-B: PEX pipe installation guide
When you are designing a system to bring potable water into a building or routing radiant heating, choosing the correct pipe can be the difference between a system that lasts 50 years and one that fails in five. For professional plumbers and contractors, cross-linked polyethylene (PEX) has become the go-to material for modern residential plumbing and hydronic heating systems. But not all PEX is created equal. Knowing the difference between PEX-A and PEX-B and understanding when to use each is a foundational skill.
What are the benefits of PEX pipe for installers?
PEX has revolutionized the plumbing industry over the last two decades. Compared to traditional rigid piping like copper and CPVC, PEX offers several distinct advantages that directly impact labor time and material costs:
Affordability: PEX is significantly more cost-effective than copper, both in terms of raw material cost and the labor required to install it.
Flexibility and reduced leak points: Because PEX is highly flexible, it can be bent around corners and obstacles, eliminating the need for many elbows and fittings. Fewer fittings mean fewer potential leak points and faster installation.
Freeze resistance: PEX can expand and contract slightly under pressure. This flexibility makes it much more resistant to bursting in freezing temperatures than rigid materials like copper or CPVC.
Corrosion resistance: PEX is immune to the mineral buildup and corrosion that can plague metal pipes in areas with hard or highly acidic water.
Types of PEX pipe
While all PEX pipes meet the same foundational standards, the letters A and B refer to the manufacturing methods used to cross-link the polyethylene. This cross-linking process defines the pipe’s flexibility, shape memory, and strength.
PEX-A
PEX-A is manufactured using the peroxide (or Engel) method. This process bonds the polymer chains during the extrusion process, resulting in the highest degree of cross-linking.
Pros: PEX-A offers the greatest flexibility, making it incredibly easy to work with in tight spaces. It has strong "thermal memory," meaning if it kinks during installation, it can be repaired simply by applying heat from a heat gun, which returns the pipe to its original shape.
Cons: It is typically the most expensive PEX option and tends to have slightly lower chlorine resistance compared to PEX-B.
PEX-B
PEX-B is manufactured using the silane (or moisture-cure) method, which cross-links the material after the pipe is formed. It is the most widely used PEX tubing in North America.
Pros: PEX-B provides the highest resistance to chlorine, making it an excellent choice for municipal water systems that use heavy chemical treatments. It also has a higher burst pressure than PEX-A and is generally the most budget-friendly option.
Cons: It is stiffer and less flexible than PEX-A. It does not have thermal memory; if a PEX-B pipe kinks, that section must be cut out and replaced with a fitting.
PEX-A vs. PEX-B comparison
| PEX-A | PEX-B | |
|---|---|---|
| Pipe Cost | More expensive | Moderate cost |
| Labor | Easiest/fastest to install due to its ability to bend around corners and existing infrastructure | Easy to install but requires more connections than PEX-A |
| Flexibility/Durability | Very flexible and durable, no coil memory | More rigid and higher burst pressure than PEX-A |
| Kinking | Easily repair kinks | Cut away the kink and replace the section of pipe |
| Fitting Types | Expansion, insert fittings: crimp, clamp, press, and push | Insert fittings: crimp, clamp, press, and push |
| Water Pressure | Highest, expansion fittings do not reduce interior pipe diameter, can make a 90-degree turn without connection (fewer total fittings required) | Insert fittings lower the water pressure, more connections are required to make turns |
| Typical Applications | Residential and commercial potable hot/cold water, large homes with multiple users, freeze zones, radiant floor heat, snow melt systems | Residential and commercial potable hot/cold water, oxygen barrier pipe for radiant floor heat and snow melt systems, DIY homeowners |
| Required Tools | Crimping tool, battery-operated expansion tool | Crimping tool, clamp/cinch tool |
| Shop Now | Shop PEX-A pipe | Shop PEX-B pipe |
PEX pipe color code
PEX tubing is commonly sold in three primary colors to help contractors instantly identify water lines:
- Red PEX: Designates hot water supply lines.
- Blue PEX: Designates cold water supply lines.
- White PEX: Can be used for both hot and cold water, often serving as main supply lines or in systems where color-coding isn't necessary. The color difference is purely visual; the structural integrity is identical across the three colors.
PEX print stream
The string of numbers and letters on the outside of the pipe is required by standards to ensure consistency. A typical print stream includes:
- Manufacturer and pipe size: Displays the brand and the standard copper tube size (CTS).
- Material designation code (PEX): A four-digit code detailing the pipe's resistance to chlorine, ultraviolet (UV) light, and its Hydrostatic Design Stress (HDS) rating.
- First digit (chlorine resistance): Ranges from 0, meaning not tested, to 5, highest resistance, for continuous recirculation of hot chlorinated water.
- Second digit (UV resistance): Indicates how long the pipe can be exposed to sunlight. A "1" means a one-month rating, while a "3" means a six-month rating. PEX should never be installed permanently outdoors where exposed to direct UV rays.
- Third and fourth digits (HDS rating): Represent the allowable stress the pipe can tolerate. "06" means 630 psi at 73 degrees Fahrenheit.
- Plumbing code compliance: Professional installations must adhere to specific codes. Look for ASTM F876, the performance standard for PEX tubing and NSF/ANSI/CAN 61, certifying it is safe for potable water distribution systems.
PEX vs. copper vs. CPVC: A professional plumbing comparison
| Feature | PEX | Copper | CPVC |
|---|---|---|---|
| Lifespan | 40–50 years | 50–70+ years | 50–75 years |
| Flexibility | Highly flexible | Rigid | Rigid |
| Installation Speed | Very fast | Slow, requires skilled soldering | Moderate, requires priming/gluing |
| Freeze Resistance | Excellent, expands slightly under stress | Poor, prone to bursting | Poor, becomes brittle and cracks |
| Maximum Temp | Up to 180°F (at lower pressures) | Up to ~401°F | Up to 200°F |
| Corrosion/Scale | Highly resistant | Susceptible to acidic water corrosion | Highly resistant to chemicals |
| UV Resistance | Poor, must be protected from sunlight | Excellent | Poor, degrades quickly in sunlight |
| Material Cost | Low | High | Low to moderate |
PEX-A vs. PEX-B fittings
Matching the right pipe to the job site requirements ensures a reliable system and protects your reputation.
Choose PEX-A when:
- The home is located in a severe cold-weather climate where freeze-thaw cycles are a concern.
- The installation requires navigating tight spaces with short-radius bends.
- Maximizing water flow pressure is critical through the use of full-flow expansion fittings.
- You are piping a hydronic radiant floor heating system.
Choose PEX-B when:
- You are working on a large-scale residential project or repipe where budget and cost-efficiency are top priorities.
- The local municipal water supply uses heavy chlorine treatments.
- You are running long, straight supply lines that don't require extensive bending.
Ferguson makes it easy to shop online for PEX pipe, PEX fittings, and PEX tools. Log in to your account and get the plumbing supplies you need, when you need them.