Plumber performs maintenance on water filtration system underneath residential sink.
Trade Talk

Reverse osmosis vs. activated carbon water filters

When homeowners complain about the taste, odor, or safety of their drinking water, recommending the most effective solution is essential for earning their trust and securing future business. As a plumbing contractor, you are frequently tasked with improving water quality for your residential customers. Two of the most dominant and proven technologies in the residential water treatment market are reverse osmosis water filter systems and activated carbon filtration.

Understanding the mechanical and practical differences in a reverse osmosis vs. carbon filter application ensures you provide the best possible system for the specific water profile of a home.

Types of water filtration

An activated carbon filter for water excels at chemical adsorption — specifically removing chlorine, chloramines, volatile organic compounds (VOCs), and unpleasant tastes or odors. It is a high-flow solution that is very frequently used to treat the entire home at the point of entry.

Conversely, a reverse osmosis water filter system provides a much more aggressive and comprehensive level of purification. By pushing water under pressure through a tightly woven, semi-permeable membrane, it strips the water of nearly all total dissolved solids (TDS), heavy metals, arsenic, and fluoride. However, this thoroughness comes at the cost of water pressure and flow rate, making it predominantly a point-of-use solution installed at a specific sink.

Activated carbon water filter systems

Activated carbon has been a staple in professional water treatment for decades. It is reliable, highly cost-effective, and exceptionally efficient at addressing the most common municipal water complaints your customers will have.

How activated carbon works

Activated carbon works by filtering water through the chemical concept of adsorption. Carbon media is specially treated with oxygen to open up millions of microscopic pores between the carbon atoms. This process creates a truly massive surface area within a relatively small physical footprint. As the home's source water flows through the activated carbon media, chemical impurities are naturally attracted to and trapped within these tiny pores.

Despite their effectiveness, carbon water filters have certain limitations. Activated carbon is exceptionally effective at removing chlorine, sediment, pesticides, herbicides, and bad tastes. However, it does not remove dissolved minerals, salts, or dangerous heavy metals like lead and arsenic. Therefore, it drastically improves the aesthetic quality of the water but is not designed to be a comprehensive purifier for highly contaminated sources.

When to use activated carbon

For residential plumbing applications, an activated carbon whole house water filter is often the ideal recommendation for customers on municipal water supplies. Here is when you should specify this option:

  • Addressing chlorine taste and odor: Municipalities heavily chlorinate water to keep it safe during transit. Carbon effectively neutralizes this chemical before it reaches the home's taps, resulting in bottled-quality water for bathing and drinking.

  • Protecting plumbing infrastructure: Constant exposure to chlorine can degrade rubber seals, toilet flappers, gaskets, and even certain plastic piping over time. A whole-house carbon system protects the home's internal plumbing components and extends the life of water-using appliances.

  • High flow rate demands: Because carbon filtration media does not significantly restrict water flow, it is perfect for treating water at the point of entry without causing frustrating pressure drops at the showerhead or kitchen sink.

  • Job scenario: A family in a suburban neighborhood on city water complains that their tap water smells strongly like a swimming pool and dries out their skin. They have no major hard water issues and their water tests negative for heavy metals. An activated carbon whole house water filter installed at the main water line is the perfect, high-flow solution to instantly improve their water quality at every fixture in the house.

Best activated carbon water filter

Selecting the best activated carbon water filter for a project depends heavily on the square footage of the home, the number of bathrooms, and the peak gallons per minute (GPM) required by the household. For a highly effective, high-capacity option, we recommend the Atlas Filtri Carbon Block CTO Reduction Filter Cartridge. This 5-micron carbon block is expertly designed to reduce chlorine, bad tastes, and odors while maintaining a steady flow rate, making it a reliable choice for whole-house applications.

Ferguson provides access to trusted brands and commercial-grade carbon filtration systems that are easy for contractors to install and service.

Shop Carbon Filters

Reverse osmosis water filter systems

When a customer's water supply contains heavy metals, high TDS, or potentially dangerous microscopic contaminants, carbon alone is simply not enough. This is exactly where reverse osmosis (RO) becomes the necessary specification.

How reverse osmosis filtration works

Reverse osmosis water filter technology is a rigorous, multi-stage purification process. The system typically begins with a standard sediment pre-filter and a carbon pre-filter. These initial stages are crucial to remove larger particles and chlorine, which would otherwise easily damage the delicate RO membrane.

The core of the system is the semi-permeable membrane itself. The home's standard water pressure forces water through this membrane, which features pores as small as 0.0001 microns. This microscopic filtration allows only pure water molecules to pass through, while actively rejecting up to 99% of dissolved solids, heavy metals, cysts, and fluoride. The rejected contaminants are safely flushed down the drain as wastewater. Finally, the purified water is stored in a pressurized holding tank and runs through a final polishing post-filter immediately before reaching the dedicated drinking faucet.

When to use reverse osmosis

Because the RO process inherently restricts water flow and produces wastewater, a reverse osmosis water filter whole house installation is exceedingly rare. Whole-house RO requires large, expensive holding tanks and powerful repressurization pumps to supply the home. Instead, the industry-standard application is a reverse osmosis water filter under sink system.

  • Ultimate drinking water purity: Recommend RO when customers demand the absolute highest quality drinking and cooking water possible, free of almost all impurities.

  • Well water applications: Homes on private wells with heavy agricultural runoff, high nitrates, or dangerous heavy metals require the intense filtration that only RO can provide.

  • High TDS municipal water: In geographical areas where city water is biologically safe but heavily laden with dissolved solids, RO is the only reliable way to bring TDS levels down to an ideal, palatable range.

  • Job scenario: A customer in an older home discovers trace amounts of lead in their tap water and wants a guaranteed safe drinking source for their young family. A reverse osmosis water filter installed directly in the kitchen provides dedicated, incredibly safe drinking water without the massive expense and space requirements of a whole-house purification setup. Remind your customers that routine reverse osmosis filter replacement is absolutely required to maintain this level of performance, which provides a great recurring revenue and service opportunity for your plumbing business.

Best reverse osmosis water filter

The best reverse osmosis filter will offer a high-efficiency membrane to reduce the amount of wastewater produced, a compact footprint to easily fit under modern, crowded kitchen sinks, and accessible, quick-change cartridges for easy service.

For a reliable replacement or upgrade component, we recommend the Atlas Filtri OASIS DP RO Membrane. This high-efficiency membrane delivers a steady 50 gallons per day of purified water, effectively stripping dissolved solids and heavy metals to provide the pristine drinking water your customers expect.

Ferguson carries industry-leading reverse osmosis water filter systems specifically tailored for professional installation.

Shop Reverse Osmosis Filters

Reverse osmosis vs. carbon filter comparison chart

FeatureActivated CarbonReverse Osmosis
Contaminants removedChlorine, chloramines, VOCs, bad tastes, odorsTDS, heavy metals, fluoride, arsenic, lead
Installation typeFrequently whole-house (point-of-entry)Primarily under-sink
Water flowHigh flow, minimal pressure dropLow flow, requires a pressurized storage tank
MaintenanceMedia replacement every 1-3 yearsFrequent pre/post filter and membrane changes
WastewaterNoneYes, varies greatly by system efficiency

The ultimate decision between a reverse osmosis vs. activated carbon setup comes down to accurately assessing the source water quality and understanding the customer's specific household goals. Activated carbon is an exceptional, reliable choice for whole-house aesthetic improvements and vital chlorine removal. Meanwhile, reverse osmosis remains the ultimate safeguard for pristine, zero-compromise drinking water at a single tap.

Often, the absolute best approach for a premium home is specifying both — a whole-house carbon filter to protect the plumbing infrastructure, paired directly with an under-sink RO system for flawless drinking water. Rely on our highly knowledgeable associates at Ferguson to help you source the exact water filtration system you need to tackle any challenging water quality job.