UV-C light for HVAC systems: Installation & maintenance guide
Integrating an HVAC UV light system offers proven air-cleaning capabilities and drastically improves overall coil efficiency over the life of the equipment. Offering these systems not only addresses the immediate health and comfort needs of customers but also establishes a reliable avenue for recurring annual maintenance and service calls.
Understand the core benefits, installation protocols, and maintenance requirements of UV-C technology, helping you communicate its value effectively and ensure safe, code-compliant installations.
The role of UV-C in HVAC
A UV-C light utilizes ultraviolet radiation — specifically in the C-band spectrum — to neutralize biological contaminants like mold, mildew, bacteria, and viruses. When applied as an AC UV light, the radiation penetrates the cellular walls of these microorganisms, rendering them inactive and unable to reproduce. In a typical UV HVAC setup, the light is strategically placed to either keep the evaporator coil clean or treat the moving air in the ductwork. By eliminating microbial growth on the coil, a UV air conditioner or furnace light restores optimal airflow and heat transfer, ultimately saving customers money on monthly energy costs and preventing premature mechanical failures.
How to install UV lights in an AC or furnace
Executing a safe and compliant installation of a UV light furnace or AC system requires careful planning and attention to detail. Proper placement, power wiring, and material protection are essential for system longevity and overall safety.
Understanding ASHRAE and IEC UV safety codes
Before drilling any access holes, it is critical to understand the governing standards that ensure both the efficacy and safety of UV-C installations.
ASHRAE Standards 185.1 and 185.2: These guidelines dictate the testing methods for UV-C lights in HVAC systems. Standard 185.1 focuses on evaluating the inactivation of airborne microorganisms in ductwork, while 185.2 addresses the intensity of surface irradiation on coils. To meet ASHRAE recommendations for effective coil sterilization, the UV light should typically deliver irradiance levels of 50 to 100 µW/cm² to the targeted coil surface.
IEC 62471-6 and IEC 60335-1: The International Electrotechnical Commission (IEC) standard 62471-6 governs the photobiological safety of ultraviolet lamp products. This standard classifies UV lights into risk groups based on their potential to cause eye damage (such as photokeratitis) or skin erythema. Furthermore, IEC 60335-1 addresses the safety of electrical appliances, explicitly detailing the protection and testing of electrical insulation that is frequently exposed to UV-C radiation.
For an installer, adhering to these codes means the installation must completely shield occupants and service technicians from direct UV exposure. This requires the mandatory use of safety interlock switches on access panels, appropriate product safety labeling, and the deliberate protection of all vulnerable internal HVAC components from prolonged radiation.
Determine optimal placement
For coil sterilization, position the UV-C light so it bathes the maximum surface area of the evaporator coil and the condensate drain pan. Ensure the light does not shine directly on non-UV-resistant plastics, as prolonged exposure to UV-C radiation will rapidly degrade certain materials, leading to cracked drain pans, brittle wire insulation, and crumbling flex duct inner liners.
Protect vulnerable materials
If the light must be installed near standard plastics, wrap the vulnerable components securely with high-quality UV-resistant aluminum foil tape or install a custom metal shield. This is a crucial step in all UV light applications to prevent secondary damage to the HVAC unit over the years.
Mount the hardware safely
Using a step drill bit or hole saw, create the appropriate access hole in the plenum or ductwork. Secure the mounting plate with self-tapping screws, ensuring an airtight seal to prevent conditioned air from escaping into the mechanical room or attic. Always ensure the light cannot be viewed directly by the naked eye during operation, as UV-C radiation is harmful to human tissue.
Wire the UV light ballast
Most residential UV lamps operate on a 24V or 120V power supply. If tapping into the furnace control board, ensure the transformer has enough available volt-amps (VA) to handle the additional load of the UV light ballast. Overloading a standard 40VA transformer is a common error that can cause the main HVAC system fuse to blow, resulting in a frustrating callback. If necessary, install a dedicated secondary transformer. Ensure all high and low-voltage wiring is routed safely away from sharp metal edges and heat sources.
UV lamp maintenance
A major advantage of offering UV systems is the built-in recurring revenue from annual maintenance agreements. While the HVAC equipment itself requires seasonal upkeep, the UV components also demand regular attention to remain effective.
How do you maintain a UV light?
Proper maintenance involves more than just swapping parts. During your routine service calls, follow these essential steps:
Clean the lamp: Dust and particulate debris can easily settle on the quartz glass of the bulb, drastically reducing its UV-C output. Wipe the bulb carefully with a soft cloth and rubbing alcohol. Avoid touching the glass with bare hands, as skin oils can create thermal hot spots that severely shorten the bulb's lifespan.
Inspect safety features: Verify that the viewport safety glass, if equipped, is fully intact and that any access panel safety interlock switches are functioning correctly to protect homeowners and future technicians.
Check the mounting and seals: Ensure the unit remains securely fastened to the ductwork and that the surrounding foil tape or mastic is properly sealed against air leaks.
UV bulb replacement
Most standard UV-C lamps lose about 15% to 20% of their germicidal intensity after 9,000 hours (approximately one year) of continuous use. Even if the bulb still visibly glows blue, its effective, invisible UV-C output has likely diminished below acceptable levels. Standard UV bulb replacement should occur annually for continuous coil-mounted systems, while some high-output or cycling airstream lamps may last up to two years. Educate customers on this specific timeline to secure ongoing service agreements and guarantee optimal air quality.
How to test a UV light ballast
If a customer reports that their UV light is out, or you notice it during a maintenance visit, the issue may lie with either the bulb or the ballast. Knowing how to test a UV light ballast saves valuable diagnostic time and prevents unnecessary part replacements.
Verify incoming power: Use an electrical multimeter to check the voltage at the input terminals of the ballast. Ensure it matches the required input (e.g., 24VAC or 120VAC). If there is no power, trace the wiring back to the transformer, switch, or control board.
Inspect the connections: Ensure the pin connectors linking the ballast to the bulb are clean, tight, and entirely free of oxidation or electrical arcing marks.
Test the output: With a known, verified working bulb installed, check if the lamp strikes successfully. If the incoming voltage is correct but the known-good bulb fails to light, the internal electronic components of the ballast have likely failed, and the entire ballast assembly must be replaced.
Maximizing the potential of HVAC UV lights
Integrating UV-C technology into residential and commercial HVAC systems is a highly effective, profitable way to improve indoor air quality and protect the structural integrity of the evaporator coil. By mastering the installation techniques — including proper strategic placement and vital material protection — and leveraging the annual UV bulb replacement cycle, contractors can provide immense value while organically growing their service business.
Ferguson is dedicated to supporting your business with the right products, rapid availability, and knowledgeable associates. Shop online for a complete inventory of UV lamps, replacement cells, and installation accessories to ensure your next job is completed smoothly and professionally.