Plumber installing ABS pipe in residential home with Milwaukee tools and Ferguson box in the background.
Trade Talk

ABS vs. PVC pipe for plumbing applications

When designing or installing drain, waste, and vent (DWV) piping, professional contractors frequently face a standard material decision: ABS vs. PVC pipe. Both acrylonitrile butadiene styrene (ABS) and polyvinyl chloride (PVC) are highly durable thermoplastic materials that have completely replaced older cast iron and lead systems in modern plumbing. They are lightweight, highly resistant to corrosion, and offer excellent, frictionless flow characteristics for wastewater. However, the choice between them is not simply a matter of preference.

Contractors must critically evaluate local building codes, extreme environmental conditions, and the specific structural requirements of the job site. Selecting the right piping material ensures a resilient installation, reduces the likelihood of callbacks, and provides long-term reliability for your customers.

ABS vs. PVC pipe

Before diving into the detailed installation specifications, it helps to understand the baseline chemical and physical properties of each pipe material.

What is ABS pipe?

ABS pipe is easily identifiable by its solid black color. It is a rigid thermoplastic polymer widely respected for its immense structural toughness and high impact resistance. The inclusion of butadiene provides its core strength against physical shock, while acrylonitrile offers thermal stability. One notable chemical characteristic of ABS is that it contains bisphenol A, commonly known as BPA, a plastic hardening agent that contributes to its overall durability

What is PVC pipe?

PVC pipe is typically manufactured in white or dark gray. It is universally utilized across both residential and commercial plumbing applications, serving as the standard for schedule 40 DWV systems. PVC is naturally BPA-free, which often makes it the preferred, or sometimes mandated, option in jurisdictions with stringent environmental or public health regulations regarding potable water and wastewater handling. While it is highly durable, it possesses slightly more flexibility than ABS, making it easier to maneuver through complex framing and tight joist spaces. Both materials share the significant advantage of being completely immune to the rust, corrosion, and scale buildup that ultimately destroys metal pipes.

Compare ABS vs. PVC pipe

Understanding how these materials stack up against each other is essential for proper job-site application. The table below outlines the primary technical differences contractors should consider.

FeatureABS pipePVC pipe
Color identificationSolid blackWhite or dark gray
Joining processOne-step specialized cementTwo-step process with purple primer and cement
Structural rigidityHighly rigid, resists extreme impactModerately flexible, easier to maneuver
Acoustic propertiesTransfers more noise from flowing waterExcellent sound dampening capabilities
Temperature tolerancePerforms exceptionally well in extreme coldBetter suited for moderate indoor temperatures
Chemical makeupContains BPABPA-free
Code acceptanceRestricted in certain local jurisdictionsWidely accepted in almost all building codes

Installation differences and serviceability

One of the most significant differences between ABS vs. PVC pipe lies in the installation and bonding process. Labor time is a critical overhead factor for any contractor, and the joining methods for these plastic pipes directly impact the speed and efficiency of the job.

ABS pipe offers a streamlined, one-step bonding process. Contractors only need to apply a specialized ABS solvent cement directly to the pipe and the fitting. The cement rapidly melts the surface layer of the plastic, creating a permanent chemical weld without the need for an additional primer. This single-step process saves valuable time on large commercial drain installations or extensive residential rough-ins, allowing crews to move to the next phase of the project faster.

Conversely, PVC pipe requires a strict, two-step joining process. Installers must first apply a chemical primer — often dyed purple to allow for quick visual inspection by code enforcement — to clean, degloss, and soften the PVC surface. Once the primer is applied and properly flashed, the PVC solvent cement is added to form the structural bond. While this process takes slightly longer and requires carrying two chemical products, it creates an incredibly secure and reliable joint. Furthermore, if an inspector demands visual proof of proper cementing, the purple primer residue on PVC joints leaves no room for ambiguity.

When it comes to serviceability, both pipes can be cut easily with standard plastic tubing cutters, reciprocating saws, or handsaws. Repairing a damaged section involves cutting out the compromised pipe and utilizing transition couplings or standard slip fittings.

How to connect ABS to PVC

During renovations and additions, contractors frequently encounter situations where they must tie a new plumbing extension into an existing drain, waste, and vent system. This often brings up the question of how to safely connect ABS to PVC. It is a critical technical issue, as improperly joining these two dissimilar plastics can lead to catastrophic joint failure and costly water damage for your customers.

Because ABS and PVC possess different chemical structures, standard solvent cements will not create a permanent, molecular bond between them. While there are special "green" transition cements available on the market designed for this purpose, many local building codes strictly prohibit their use due to long-term failure rates. The most reliable and universally code-compliant method for transitioning between ABS vs. PVC pipe is utilizing a mechanical coupling. Flexible rubber transition couplings, secured with heavy-duty stainless-steel bands, create a watertight, secure seal. This mechanical method also accommodates the slightly different expansion and contraction rates of the two plastics, ensuring a professional-grade connection that will stand the test of time.

ABS vs. PVC pipe performance

The environment where the piping will be installed heavily dictates which material will perform best over the decades. A critical rule for both plastics is that neither ABS nor PVC should be stored outdoors or installed in areas with prolonged exposure to direct sunlight. Ultraviolet (UV) rays actively degrade the plastic polymers over time, causing them to become brittle and prone to shattering. If outdoor, above-ground installation is absolutely unavoidable, both pipe types require a thick protective coating of UV-resistant, water-based latex paint to shield the material.

In underground applications, particularly in regions that experience harsh winters, ABS is often considered the superior choice. Its rigid composition and structural toughness allow it to withstand shifting soil loads and extreme cold without fracturing. Plumbers frequently choose ABS for underground sewer lines because it resists the physical shock of trench backfilling and the stress of freezing ground temperatures better than alternative plastics.

PVC, however, holds a distinct advantage indoors, primarily due to its acoustic properties. PVC naturally dampens the sound of running water significantly better than the rigid walls of ABS. When plumbing a heavy drain line through a residential living room wall or between open-concept floors, using PVC ensures that your customers will not be continuously disturbed by the noise of wastewater traveling through the pipes. PVC is also highly resistant to chemical degradation, making it suitable for a wide variety of commercial waste applications, including salons or light industrial spaces where chemical disposal is common.

When to choose each option

Every job site presents unique structural and environmental challenges. Here are the specific scenarios where a contractor should choose one material over the other to guarantee the best results.

ABS plumbing applications

  • Underground sewer installations: Its exceptional impact resistance makes it ideal for handling heavy, compacted soil loads and trench backfilling without cracking.
  • Extreme cold environments: ABS maintains its structural integrity and resists shattering in freezing temperatures far better than PVC.
  • Time-sensitive projects: The primerless, one-step cementing process significantly reduces labor time on extensive DWV pipe runs.
  • Commercial drain retrofits: The raw durability of ABS provides peace of mind in high-traffic commercial environments where exposed pipes might be subjected to accidental physical stress or impact.

PVC plumbing applications

  • Indoor residential plumbing: The superior sound-dampening qualities of PVC ensure a quiet drainage system, which is a major comfort factor for residential customers.
  • Areas with strict building codes: Because PVC is entirely BPA-free, it faces fewer regulatory hurdles and is universally accepted in almost all municipalities across the country.
  • Complex routing and framing: The slight inherent flexibility of PVC allows contractors to maneuver the pipe more easily through tight spaces and restrictive floor joists.
  • Projects requiring clear inspection verification: The mandatory use of purple primer provides immediate visual confirmation that joints are properly prepared, satisfying local plumbing inspectors quickly and keeping the job moving.

By understanding the distinct advantages, chemical properties, and installation methods of both ABS and PVC, contractors can make informed decisions that ensure leak-free installations. Shop high-quality pipes, fittings, and cements for your next project at Ferguson or explore more in our Ideas and Learning Center.