How to resolve failing heat pump reversing valves
When servicing a heat pump that is not heating or cooling properly, diagnosing the root cause can quickly become a complex process. Both a bad compressor and a bad reversing valve share similar symptoms. However, misdiagnosing the issue costs you time and your customers money. Understanding how to definitively test and isolate a reversing valve failure is a critical skill for any HVAC professional.
Reversing valve operation
To properly diagnose a problem, it is important to first understand the heat pump reversing valve location and its normal operation. Typically located inside the outdoor condenser unit, this four-way valve is responsible for switching the direction of the refrigerant flow. This allows the system to change between heating and cooling modes.
The valve consists of a main body with a sliding mechanism, a smaller pilot valve, and the heat pump reversing valve solenoid. When the thermostat calls for a mode change, 24 volts are sent to the solenoid. The energized coil creates a magnetic field that moves the pilot valve. This movement changes the pressure dynamics inside the valve body, utilizing the system's refrigerant pressure — which generally requires a 30 to 70 PSI differential — to push the internal slider to the opposite side.
Symptoms and causes of a bad reversing valve
When a reversing valve malfunctions, it generally exhibits one of two primary behaviors: it gets physically stuck, or it leaks internally. Isolating whether the issue is electrical or mechanical will dictate your next steps.
Electrical problems
Many times, a reversing valve failure is actually an electrical issue rather than a failure of the mechanical valve body. If the thermostat is calling for a mode change but the valve does not shift, the system will present as a reversing valve stuck in heat mode, or cooling mode, depending on the brand default.
Electrical causes typically point to a failed heat pump reversing valve solenoid coil, a broken control wire, a bad defrost control board, or an issue with the thermostat. If the coil burns out, it will no longer create the magnetic field necessary to move the pilot valve, leaving the system stranded in its default position.
Mechanical problems
If the electrical components are functioning correctly, the issue is mechanical. Mechanical problems generally fall into two categories: a physically stuck valve slider or an internal leak.
A stuck slider can happen due to debris in the refrigerant lines, a lack of use during mild seasons, or an improper refrigerant charge that fails to create the pressure differential needed to move the slider.
An internal leak, or "bleeding," occurs when the internal slider does not seat properly or the internal seals degrade. Refrigerant bypasses the proper channels, leaking directly from the high-pressure side to the low-pressure side. This causes poor performance in both heating and cooling modes.
Reversing valves: Diagnosing electrical vs. mechanical issues
| Failure type | Common symptoms | Diagnostic test | Repair action |
|---|---|---|---|
| Electrical | System stuck in default mode, no click heard when switching modes | Verify 24V at coil, perform magnetic screwdriver test | Heat pump reversing valve solenoid replacement |
| Mechanical (Stuck) | System stuck in one mode, coil has strong magnetic pull | Cycle modes rapidly, tap valve body | Unstick valve or replace complete valve body |
| Mechanical (Leak) | Poor heating and cooling capacity, hissing sound | Temperature differential test on suction lines | Replace complete valve body |
Testing the heat pump reversing valve solenoid
Before condemning the entire valve body, you must rule out the electrical components. This requires a reliable multimeter and a standard steel screwdriver.
- Verify voltage: Ensure the thermostat is calling for the non-default mode. Use your multimeter to check for 24V at the solenoid coil. If you do not have voltage, the issue is likely the thermostat, the defrost control board, or broken wiring.
- Check the coil resistance: If voltage is present, turn off the power and check the coil for continuity. It is crucial to understand your multimeter readings here: an "OL" (Over Load or Open Loop) reading indicates an open circuit, meaning the internal wire is broken and the coil is burnt out. A 0.00 (zero) reading indicates a short circuit, meaning the coil's resistance is completely gone. In either case, if the reading is not showing the manufacturer's specified resistance, the coil is defective.
- The magnetic test: If you have voltage and the coil has continuity, restore power and hold a steel screwdriver near the center of the coil. You should feel a distinct magnetic pull. If the magnetic field is weak or absent, the solenoid is defective.
How to unstick a reversing valve
If the electrical tests pass, but the valve still refuses to shift, the internal slider may be physically jammed. This can happen due to debris in the lines, a lack of use during mild seasons, or low refrigerant charge.
Knowing how to unstick a reversing valve can occasionally save your customers from needing an immediate and costly repair. First, try cycling the system from heat to cool multiple times at the thermostat or control board. The sudden shifts in pressure can sometimes break the slider free.
If that does not work, locate the main body of the valve. Using a soft, rigid object — like the plastic handle of your screwdriver — gently tap on the sides of the valve body while the system is attempting to shift. Never strike the valve with a hammer or a metal wrench, as this will dent the brass casing or crush the delicate capillary tubes, guaranteeing the need for a full replacement. If the gentle tapping frees the valve, monitor the system for a few cycles. If it sticks again, replacement is necessary.
Diagnosing an internal reversing valve leak
An internal leak, or "bleeding," occurs when the internal slider does not seat properly or the seals degrade. Refrigerant bypasses the proper channels, leaking directly from the high-pressure side to the low-pressure side. This causes poor performance in both heating and cooling modes, mimicking a failing compressor.
To check for an internal leak, run the system for about ten minutes to stabilize pressures. Using accurate pipe temperature clamps, measure the temperature of the true suction line and compare it to the suction line coming from the evaporator. A properly functioning valve should have a temperature differential of 3 degrees Fahrenheit or less. If the difference is greater than 3 to 5 degrees, refrigerant is bleeding across the valve, and it must be replaced.
Differentiating between a bad reversing valve and a failing compressor
A reversing valve that is bleeding internally shares symptoms with a compressor that has bad internal valves. In both scenarios, the system will show lower than normal head pressure and higher than normal suction pressure. Because a compressor replacement is a significantly larger investment for your customers, you must confirm which component has failed.
If the temperature differential test across the reversing valve shows a difference of more than 3 degrees, the reversing valve is the culprit. If the temperatures across the suction ports are virtually identical, but the system pressures are still equalizing while the compressor is running, the compressor's internal valves are likely damaged. Performing a pump-down test — where applicable and safe for the specific compressor type — can further verify the compressor's mechanical health.
Heat pump reversing valve solenoid replacement and valve repair
Whether you are swapping a coil or brazing in a new valve body, utilizing the proper tools and techniques ensures a reliable repair.
Replacing a bad reversing valve solenoid
If your diagnostics point to a dead coil, a heat pump reversing valve solenoid replacement is a quick and straightforward job that does not require opening the refrigerant circuit.
- Disconnect all power to the condenser unit.
- Remove the retaining nut or clip holding the solenoid coil to the pilot valve stem.
- Slide the old coil off the stem.
- Disconnect the wiring leads, taking note of their routing.
- Slide the new coil onto the stem and secure the retaining nut.
- Connect the new wiring leads, restore power, and test for proper operation.
Replacing a bad reversing valve
Replacing the entire reversing valve is a labor-intensive task that requires precision. Because the valve body is constructed of brass and contains sensitive internal nylon or Teflon components, heat management during brazing is the most critical aspect of the job.
- Safely recover all refrigerant from the system.
- Unbraze or cut the old valve out of the system. Cutting is often preferred if space allows, as it prevents drawing old, contaminated oil and debris back into the lines.
- Prepare the new valve and the existing copper lines by cleaning them thoroughly.
- Protect the new valve: This step is non-negotiable. You must wrap the body of the new reversing valve with soaking wet rags or apply a commercial heat-blocking gel.
- Braze the connections quickly and efficiently, directing the torch flame away from the valve body. Re-wet the rags between brazing each joint. If the body of the valve gets too hot, the internal seals will melt, and the brand-new valve will fail immediately upon startup.
- Install a new bi-flow liquid line filter drier.
- Pressure test the system with nitrogen, pull a deep vacuum, and recharge the system with virgin refrigerant to factory specifications.
Partnering with Ferguson for your HVAC needs
Accurate diagnostics and proper repair techniques separate top-tier technicians from the rest. When dealing with a reversing valve failure, taking the time to test electrical vs. mechanical components ensures you provide the most accurate and cost-effective solution for your customers.
When you need a replacement reversing valve, solenoid, or the tools to get the job done right, rely on Ferguson and keep your trucks stocked and your business moving forward.