Hot water recirculating system design & installation
Eliminating the wait for hot water is a frequent and high-priority request from customers. Waiting for hot water wastes thousands of gallons of water annually and causes noticeable frustration in both residential and commercial settings. Installing a hot water recirculating system is the industry-standard solution. By keeping hot water staged close to the fixtures, these systems deliver immediate comfort while conserving valuable water resources.
Explore hot water recirculation system design and evaluate dedicated return loops, crossover retrofit systems, and modern integrated-pump water heaters. Understanding how these distinct technologies differ ensures you deliver the optimal solution, balancing installation labor, material costs, and long-term energy savings for your customers.
What is a recirculating pump?
A hot water circulation pump is a specialized, fractional-horsepower motorized device that moves hot water from the water heater through the supply pipes and back again. This continuous movement ensures hot water is always stationed near the plumbing fixtures, ready for immediate use.
How does a hot water recirculating system work as a complete assembly?
Recirculation systems rely on creating a closed loop. This loop can be formed by installing a dedicated extra return pipe, or by using the existing cold water line as a temporary return path. Regardless of the method, proper domestic hot water recirculation pump control is critical. Without controls, the pump runs endlessly, forcing the water heater to fire constantly. This wastes energy, inflates utility bills, and accelerates copper pipe erosion due to constant water velocity.
How does a hot water recirculating pump work?
Hot water recirculation pumps create a slow, continuous, or intermittent flow within the plumbing circuit, overcoming the static pressure of the water in the pipes. When a user opens a tap, the hot water is already present at the valve.
Designing a hot water recirculating system
When selecting and installing hot water recirculation system components, contractors generally choose between two primary designs. Each approach has unique structural requirements and performance outcomes.
Hot water recirculating system with dedicated return line
A dedicated system involves running an additional, dedicated pipe from the furthest plumbing fixture back to the water heater. The recirculating pump is typically installed on this return line, located near the tank or tankless unit. A hot water recirculating system with dedicated return line diagram usually illustrates a complete physical loop, offering the most reliable and balanced water pressure.
This setup is highly efficient and keeps the hot and cold water streams entirely separate. However, it requires significant labor and material to run the extra piping, making it best suited for new construction, extensive renovations, or total repipes.
Hot water recirculating system without dedicated return line
For retrofits in existing structures, opening walls to run a new return pipe is often cost-prohibitive and impractical. A hot water recirculating system without a dedicated return line utilizes a thermal bypass valve, or crossover valve, installed under the sink at the furthest fixture. The pump, often located directly at the water heater, pushes hot water into the main supply line.
The bypass valve allows the cooling water at the end of the line to cross over into the cold water line and return to the water heater. Once the hot water reaches the valve and heats the internal thermostatic element, the valve closes. This method requires significantly less labor but can cause a short burst of warm water when customers initially open the cold tap.
Dedicated vs. non-dedicated return lines for hot water circulation
| Recirculation System type | Installation labor | Best applications | Water line impact | Initial cost impact |
|---|---|---|---|---|
| Dedicated return line | High, requires extra piping | New construction and full repipes | Keeps hot and cold streams entirely separate | Higher due to extended labor and materials |
| Without dedicated return line | Low, uses thermal bypass valve | Retrofits and targeted remodeling | Temporarily warms the cold water line | Lower, due to faster installation |
Choosing hot water recirculation controls and parts
Selecting the right hot water recirculation control device is a critical step in the installation process as continuous water velocity and turbulence isn't the most efficient and can cause pinhole leaks.
- Timer for hot water recirculating pump: Using a timer is a simple, analog, and cost-effective method. Timers ensure the pump only runs during peak usage hours — such as early mornings and evenings — preventing energy waste during the middle of the night or workday.
- Aquastats: These mechanical or digital temperature sensors shut off the pump when the return line reaches a predetermined set temperature. Once the line cools down, the aquastat triggers the pump to run again, ensuring the line remains primed with hot water without running continuously.
- Smart demand triggers: Push buttons, flow switches, or motion sensors activate the pump only when a user actively needs hot water. This on-demand approach provides the highest level of energy efficiency and is often required to comply with strict modern energy codes.
Benefits of hot water recirculation
For contractors, recommending a hot water recirculation system is an excellent way to provide immediate, tangible value to your customers. Understanding the primary benefits helps in positioning these systems effectively during consultations, routine service calls, or new construction bids.
- Significant water conservation: The most measurable and immediate benefit is the massive reduction in water waste. Waiting for hot water can waste up to 12,000 gallons of water annually in a typical household. Recirculating systems completely eliminate this clean water runoff down the drain, making them an eco-friendly upgrade that appeals heavily to environmentally conscious customers and helps regions facing severe water scarcity.
- Unmatched convenience and comfort: Customers ultimately want luxury and efficiency in their everyday spaces. Providing zero-wait hot water at every plumbing fixture — from the kitchen sink to the primary bathroom shower — drastically improves their daily routine. It eliminates the frustration of standing in a cold bathroom waiting for the shower water to warm up.
- Enhanced energy efficiency: While it may seem counterintuitive that running an electric pump saves energy, utilizing the correct smart controls prevents the water heater from firing unnecessarily. By only running the pump when needed, the system minimizes standby heat loss in the pipes and reduces overall utility bills compared to continuous operation or constantly replacing dumped hot water.
- Plumbing system longevity: Traditional non-recirculating systems experience significant thermal expansion and contraction every time hot water surges through cold pipes and then rapidly cools down. A properly designed recirculation system maintains a much more consistent baseline temperature, reducing thermal stress and physical movement on the piping infrastructure over its lifespan.
Deliver comfort with Ferguson
Hot water recirculation systems offer a tangible, high-value upgrade to everyday living, conserving vital water resources and elevating overall home comfort. Whether you need a simple timer-controlled pump or a high-efficiency integrated tankless water heater, Ferguson provides the expansive local inventory and dedicated support required for your next project. Shop recirculation pumps and ensure you have the right equipment for any residential or commercial application.