Refrigerant leak detection: Best practices & tools
For professional HVAC contractors, finding and repairing refrigerant leaks is one of the most critical aspects of maintaining a healthy, efficient system. A unit that is low on refrigerant forces the compressor to work harder, consuming excess energy and dramatically increasing the likelihood of premature failure. With the ongoing phasedown of hydrofluorocarbons (HFCs) and the transition to newer refrigerants, the cost of replacing lost refrigerant is rising sharply. The Environmental Protection Agency (EPA) also strictly enforces Section 608 regulations, which mandate regular leak inspections and timely repairs for systems above specific charge weights.
To stay compliant and protect your customers' investments, you need the right diagnostic tools. While visual inspections and leak detection soap still have their place, electronic refrigerant leak detectors are the modern standard for fast, accurate troubleshooting. However, the technology inside your detector matters more than most technicians realize.
In this comprehensive guide, we will break down the fundamental differences between the three main types of electronic leak detectors: heated diode, electrochemical, and infrared. We will cover their pros and cons, discuss their compatibility with mildly flammable A2L refrigerants, and review the best practices that will help you find micro-leaks with confidence.
Types of refrigerant leak detectors
If you need to make a quick purchase decision, understanding the baseline differences between these sensor technologies is the first step. Here is a brief comparison of how these electronic leak detectors stack up against one another:
| Technology | How it works | Sensor life | False alarm risk | Upfront cost |
|---|---|---|---|---|
| Heated diode | Heat ionizes halogen gases, changing electrical current. | 100 to 300 hours | Moderate | Lower |
| Electrochemical | Target gas causes a chemical reaction, generating a signal. | Varies by gas | Low to moderate | Low to moderate |
| Infrared | Measures infrared light absorption by specific gases. | Up to 10 years | Very low | Higher |
Heated diode leak detectors
Heated diode detection is the technology that built the professional HVAC leak detector market, and it remains the dominant approach for residential and light commercial work.
How they work
At the core of a heated diode detector is a small ceramic element that is electrically heated to a high temperature. A small internal pump draws ambient air across this element. When halogen-based refrigerants — such as common CFCs, HCFCs, and HFCs — contact the heated tip, the molecules break apart. This creates positively charged fluorine and chlorine ions, which generate an electrical current that triggers the detector's alarm.
Pros of heated diode
- Stationary pinpointing: Unlike some newer technologies, heated diode detectors measure absolute concentration. This means you can move to the spot of a suspected leak and hover the probe directly over a flare fitting or valve to pinpoint the exact location.
- High sensitivity: Top-tier heated diode models are exceptionally sensitive, capable of finding leaks as small as 0.03 ounces per year.
- Affordability: They offer excellent performance at a highly accessible price point, making them a staple in most HVAC technicians' tool bags.
Cons of heated diode
- Consumable sensors: The sensor degrades with excessive refrigerant exposure and naturally burns out over time. You can expect to replace a heated diode sensor after 100 to 300 hours of operation.
- False positives: These detectors can sometimes be triggered by moisture, oil, or other jobsite chemicals, leading to nuisance alarms.
- Warm-up time: The sensor element requires time to heat up before the tool can be used accurately.
Electrochemical leak detectors
Electrochemical sensors (often grouped closely with corona discharge technologies in older units) utilize a specialized internal chemical process to identify the presence of a gas.
How they work
These detectors pull sampled air through an electrical field or a specialized chemical matrix. When the target gas enters the sensor, it undergoes a chemical reaction that alters the current flow between electrodes, triggering the alarm.
Pros of electrochemical
- Gas-specific targeting: Electro chemical sensors are often designed to react to very specific gases, making them highly effective in industrial applications where a specific refrigerant (like Ammonia) is heavily used.
- Affordability: Like heated diode units, they have a lower initial cost of entry for basic models.
Cons of electrochemical
- Lifespan limitations: The chemical electrolytes within the sensor eventually deplete or dry out, necessitating frequent sensor replacements. Older corona discharge models had sensor lifespans as short as 24 hours of active use.
- Environmental sensitivity: Humidity, high winds, and dust can easily affect the accuracy of basic electrochemical and corona discharge sensors.
- False alarms: Because the electric arc breaks down various gases, older models are notorious for producing false alarms on jobsites with mixed chemical vapors.
Infrared leak detectors
Infrared (IR) leak detectors represent the premium tier of electronic leak detection. They offer unparalleled stability and longevity, making them an excellent investment for volume commercial work.
How they work
Infrared detectors do not rely on heat or chemical degradation. Instead, they shine a beam of infrared light through a sample cell containing the drawn-in air. Because different refrigerant molecules absorb infrared light at specific, unique wavelengths, the detector's optical sensor registers this absorption as a drop in signal strength and sounds the alarm.
Pros of infrared
- Exceptional sensor life: Because the sensor is not placed directly in the stream of breaking-down chemicals, it does not suffer from rapid degradation. Infrared sensors often last 10 years or more, drastically lowering the total cost of ownership.
- Minimal false alarms: Since light absorption is gas-specific, infrared detectors are highly resistant to false positives caused by jobsite solvents, oil, or temperature swings.
- Consistent sensitivity: The unit maintains its full accuracy across a broad spectrum of modern refrigerants, including newer low-chlorine blends, without degrading over time.
Cons of infrared
- Constant motion required: Infrared detectors compare air samples to one another to detect a differential in concentration. This means the probe must be moved continuously to work properly; if you stop and hover over the leak, the unit will quickly recalibrate to the new ambient concentration and stop alarming.
- Higher initial investment: The advanced optical technology inside an IR detector makes it significantly more expensive upfront than heated diode models.
Are your leak detectors ready for A2L refrigerants?
The HVAC industry is rapidly shifting toward low-GWP (Global Warming Potential) alternatives, which means A2L refrigerants like R-32 and R-454B are becoming the new standard. Because A2L refrigerants are classified as mildly flammable, many contractors worry about tool capability and safety.
A pervasive myth in the industry is that heated diode sensors are unsafe for A2L refrigerants because of their internal heating elements. This is entirely false. The heated diode sensor in a modern leak detector operates at roughly 122°F (50°C). By comparison, the ignition point of R-32 is 1,198°F (648°C).
Most modern heated diode and infrared leak detectors on the market are completely safe, A2L compatible, and will not ignite the refrigerant. Because R-32 and R-454B have high HFC content, any quality detector designed for HFCs will readily sniff them out.
HVAC leak detector selection
Choosing the best refrigerant leak detector depends entirely on your daily workload and budget.
- Choose a heated diode detector if: You primarily work on residential splits or light commercial packaged units, and you value the ability to hover over a suspect joint to pinpoint a micro-leak. It is the best choice if you prefer a lower upfront cost and don't mind changing the sensor once or twice a year.
- Choose an infrared detector if: You service large commercial VRF systems, supermarket racks, or work in environments with heavy background chemicals. The high upfront cost is quickly offset by the 10-year sensor life and the reduction in frustrating false alarms.
- Choose an electrochemical detector if: You operate in specific industrial refrigeration niches where gas-specific electrochemical sensors are required to safely monitor highly toxic substances like ammonia.
The best refrigerant leak detectors
When you are ready to upgrade your diagnostic tools, Ferguson provides access to the industry’s most trusted options. Here are our top product recommendations across technologies:
- Fieldpiece Instruments Heated Diode Refrigerant Leak Detector (DR58): An outstanding A2L-compatible choice for residential contractors. This unit detects leaks smaller than 0.1 oz/year and features a manual or automatic "zeroing" function to cancel out background contamination. It is built with a rugged boot and a 15-hour rechargeable battery.
- Fieldpiece Instruments Infrared Refrigerant Leak Detector (DR82): Built for longevity, this A2L-ready detector utilizes an infrared sensor designed to last up to 10 years. It features a large backlit LCD, a lighted LED tip for dark mechanical rooms, 10 hours of battery life, and excellent water and impact resistance.
- Yellow Jacket AccuProbe™ IR Refrigerant Infrared Leak Detector: Offering ultimate sensitivity and accuracy, the AccuProbe™ IR easily detects all CFC, HCFC, HFC, and HFO refrigerants. It is a highly dependable, A2L-compatible choice for commercial contractors working with a wide range of modern and legacy blends.
- Robinair LD5 Refrigerant Leak Detector: Made in the USA, the LD5 offers instantaneous response times with a unique 128 x 160 full-color graphic LCD display. With a long 17-inch probe, a high-intensity LED inspection light, and three adjustable sensitivity levels, it makes pinpointing leaks fast and visually intuitive.
Best practices for refrigerant leak detection on the job
Regardless of which technology you choose, a high-end leak detector is only as effective as the technician operating it. Follow these best practices to eliminate callbacks and ensure accurate diagnostics:
- Verify the leak first: Before you spend an hour scanning a massive system, use your gauges to verify that a leak actually exists. Abnormal superheat or subcooling readings will confirm a low charge before you break out the electronic sniffer.
- Zero the meter in fresh air: Always turn on your electronic leak detector outside the building in clean air. Allow it to self-calibrate before entering the mechanical room or residence.
- Follow the oil: Refrigerant oil escapes alongside the gas. Conduct a visual inspection of service valve caps, compressor terminals, filter driers, and flare fittings. Wherever you see an oil stain, start sniffing.
- Move at a snail's pace: The biggest mistake technicians make is sweeping the probe too fast. You should move the detector slowly, at a rate of roughly 2 to 3 inches per second. Sweeping too fast creates a breeze that disrupts the gas cloud before the sensor can pull a sample.
- Verify with soap bubbles: Electronic detectors are incredibly sensitive, but they cannot show you the exact physical hole. Once your heated diode or infrared detector sounds the alarm, spray the suspected joint with a high-quality micro-leak detection bubble solution. This gives you absolute, visual confirmation of the leak before you quote a repair.
- Never sniff pure refrigerant: Never open a jug of virgin refrigerant and stick your heated diode probe into the blast just to "test" if the meter works. The massive concentration of halogen gas will instantly degrade and ruin your sensor.
A reliable electronic leak detector is an indispensable part of a professional HVAC toolkit. Whether you prefer the stationary pinpointing of a heated diode, the industrial specificity of an electrochemical sensor, or the unmatched longevity of an infrared unit, understanding the underlying technology empowers you to work smarter.
When you rely on your equipment every day, downtime is not an option. Ferguson provides access to trusted brands and the latest diagnostic technologies. Whether you are replacing a fouled sensor or upgrading to an advanced A2L-ready infrared model, shopping with Ferguson ensures you have exactly what you need.