Close up imagery of water heater pressure relief valve.
Trade Talk

Water heater safety valves, tanks & pans: A plumber's guide

For professional plumbing contractors, a water heater installation is only as good as its safety measures. Whether you are setting up a commercial system or a residential tank — managing thermal expansion, pressure spikes, and potential water damage is a critical part of the job. Code compliance keeps the inspectors happy, but choosing the right safety components is what protects your customer’s property and your business's reputation.

To ensure your next installation is fully protected, here is a technical overview of the essential safety components — including temperature & pressure (T&P) valves, drain pans, and leak detection systems.

Temperature & pressure safety: T&P valves

The T&P valve is often considered the most important safety device on any water heater because it is the main defense against dangerous pressure build-up. If the thermostat breaks and the heater keeps running without stopping, the water temperature and pressure inside the tank can quickly rise to dangerous levels.

How does a pressure relief valve work?

T&P valves are designed to open and discharge water if the internal tank temperature reaches 210°F or if the internal pressure exceeds the valve's rating — typically 150 PSI for standard residential models.

How to replace a T&P relief valve

To replace a water heater temperature and pressure (T&P) relief valve:

  1. Turn off the water heater's power or gas supply and close the main cold water valve.

  2. Drain a few gallons of water out of the tank so the water level sits below the valve before unhooking the discharge line and unscrewing the old valve.

  3. Clean the tank's port threads thoroughly with a wire brush to remove any old sealant or corrosion, ensuring a flawless, leak-free seat for the new component.

  4. Wrap the threads of the new valve with plumber's tape before screwing it in tightly with the opening facing down.

  5. Hook the discharge line back up, making sure to inspect the entire line for any internal obstructions, mineral buildup, or improper scaling that could dangerously restrict flow.

  6. Turn the water supply on to refill the tank completely, and then turn the power or gas back on.

Which T&P relief valve does Ferguson recommend?

You can find various T&P relief valves in the market designed to prevent dangerous pressure buildup. Check out this T&P relief valve from PROSELECT®. It features heavy-duty brass construction, making it the industry standard for reliable water heater protection.

Protect pipes with a water heater thermal expansion tank

In closed-loop systems, a T&P valve shouldn't be your daily pressure regulator. Ferguson carries a full line of thermal expansion tanks to absorb volume changes, protecting your customer’s pipes and ensuring the manufacturer’s warranty remains valid.

Most homes use a 2-gallon or 4.5-gallon tank, depending on how big your water heater is and how high your home’s water pressure runs. Standard tanks are made of tough steel with a rubber lining inside, which works perfectly for regular tap water. If your local water has harsh chemicals or a lot of minerals that cause rust, stainless steel models are a better choice because they last longer and won't corrode.

However, an expansion tank only works if it is set up right. It needs to be installed on the cold water pipe going into the water heater. Before you turn the water on, use a transfer pump to fill the tank with enough air to exactly match your home's water pressure. If you skip this step, the rubber lining inside will pop early, and the installation won't pass inspection.

Which thermal expansion tank does Ferguson recommend?

Protecting plumbing systems from high pressure is made possible by the different thermal expansion tanks available — and this one from PROFLO® is built to meet local plumbing codes and protect your system from high pressure. It features a heavy-duty rubber lining designed to handle constant pressure changes, plus a special built-in liner that stops bacteria from growing inside the tank.

Defend floors with a water heater drain pan

Even the best water heaters have the potential to wear out without notice and leak. A heavy-duty drain pan sits under the tank to act as a first line of defense, catching leaking water before it can cause costly problems like rotted floors, structural damage, and mold growth. Plastic pans are budget-friendly and won't rust, making them great for residential electric water heaters. Metal pans, made of aluminum or galvanized steel, are more durable and required for commercial buildings or gas water heaters where high temperatures could melt plastic.

However, a drain pan only works if it has somewhere to send the water. To protect the property, you must connect a dedicated drain pipe to the pan's outlet so that any leaks are safely carried away to a floor drain, utility sink, or outside the building — in line with any local plumbing codes.

Which water heater drain pan does Ferguson recommend?

To keep leaks from damaging the floors, there’s a wide array of different drain pans available that are worth a look. This water heater drain pan from Jones Stephens® provides rugged, code-compliant containment for gas or electric installations, pre-drilled to accommodate standard drain fittings.

Advanced leak detection and automatic shutoff valves

While traditional drain pans only catch leaks in one spot, modern homes and businesses are turning to smart leak detection systems for better protection. These systems use small sensors placed in the drain pan or on the floor. The moment any moisture touches them, they instantly send out an alert, so the homeowner is made aware of a problem and can act quickly.

To stop flooding before it starts, premium systems use an automatic shutoff valve installed on the main cold water pipe. When the sensors detect a leak, the system immediately shuts off the incoming water supply and sends a notification to the homeowner or property manager. This stops the water from running continuously, limiting the damage to only what was already inside the tank.

Which leak detection system does Ferguson recommend?

You can look into a variety of leak detection systems designed for your plumbing setup. For example, Ferguson carries the Moen® Flo Smart Water Monitor & Shutoff, a smart device that is installed on the main water line. Flo by Moen will automatically turn off the water protect the home from catastrophic water damage.

Every local area has its own specific rules when it comes to plumbing codes, thermal expansion tanks, and where drain pipes are allowed to run. Don't leave your risk management to chance. Ferguson sources reliable, cutting-edge safety components from top industry manufacturers. Our knowledgeable associates can help you find the exact valves, pans, and smart monitoring systems required to keep your projects safe, compliant, and performing at their best.