HVAC technician holds flashlight while inspecting inside of furnace heat exchanger.
Trade Talk

Furnace heat exchanger diagnostics: Verifying cracks

When a customer calls about a malfunctioning heating system, checking the furnace heat exchanger is often a top priority. This component is critical for both comfort and safety in a home, serving as a barrier between combustion gases and breathable air. Finding a crack in a furnace heat exchanger requires a systematic approach, using the right tools to confirm the diagnosis and protect the household from carbon monoxide exposure. As a contractor, your customers rely on your expertise to accurately identify cracked heat exchanger symptoms and guide them toward a safe, cost-effective solution.

How heat exchangers crack

A gas furnace heat exchanger is a series of metal tubes or coils that absorb and transfer heat from the combustion process to the air blowing across them. It keeps the toxic byproducts of combustion — like carbon monoxide, sulfur dioxide, and nitrous oxide — completely separated from the air that gets circulated through the home.

When this metal barrier is compromised, it becomes a severe safety hazard. Understanding what causes a heat exchanger to crack helps you explain the root of the problem to your customers. The four most common culprits include:

  • Overheating: A clogged air filter or blocked return vents restrict airflow, trapping heat and putting the metal under immense thermal stress. This is a leading cause of a cracked heater exchanger.

  • Age and wear: The natural cycle of metal expanding as it heats and contracting as it cools will eventually cause metal fatigue over years of use.

  • Oversized furnace: A system that is too large for the ductwork will short-cycle, causing rapid temperature fluctuations that rapidly weaken the component.

  • Corrosion and rust: Excess moisture from improper condensation drainage can rust the exchanger from the inside out, leading to premature failure.

Is a cracked heat exchanger dangerous?

It is your responsibility to clearly explain the severity of the situation. A cracked heat exchanger is an immediate life safety hazard. There is no gray area to negotiate.

When carbon monoxide escapes into the supply air stream, it is distributed directly into the living spaces. Because carbon monoxide is completely colorless, odorless, and tasteless, it can cause severe illness or death before the occupants even realize there is a problem. If you confirm a crack, you must follow your local codes and company policies, which generally require disabling the heating function of the furnace and capping the gas line to prevent accidental operation. Always recommend that customers install high-quality carbon monoxide detectors on every level of their home.

Cracked heat exchanger symptoms

Being able to identify cracked heat exchanger symptoms quickly can save lives. While some signs are obvious, others require a trained eye. Always keep a close watch for these red flags during a service call:

  • Yellow or dancing burner flames instead of a steady, solid blue flame.

  • Excessive soot buildup around the burners, heat exchanger chamber, or exhaust flue.

  • A strong, putrid chemical or metallic odor near the unit.

  • The carbon monoxide detector going off in the living space.

  • Customers reporting unexplained health symptoms like chronic headaches, nausea, or sleepiness while the heat is running.

  • Water puddling near the base of the furnace, which can sometimes indicate a structural failure in high-efficiency condensing furnaces.

Verifying a cracked heat exchanger

When you suspect a hairline crack in a furnace heat exchanger, you must verify it definitively before condemning the unit. Guesswork is never acceptable when carbon monoxide is involved. There are several ways regarding how to check for a cracked heat exchanger.

Heat exchanger diagnostic methods

Diagnostic methodAdvantagesLimitationsRecommended tools
Visual inspectionDirect visual confirmation of the crack, easy to document and show to customersHairline cracks can be hidden in tight bends or only open up when the metal is hotKlein Tools Utility Borescope, flashlight, inspection mirror
Combustion analysisTests the system under real operating conditions, identifies dangerously high CO levels immediatelyHigh CO can be caused by other combustion issues, requiring further investigation to confirm a crackYellow Jacket Combustion Analyzer
Flame displacement testExtremely quick and requires no specialized equipment, good initial indicator of a problemDoes not confirm the exact location of the crack; not a definitive test on its ownNone (visual observation only)
Exchanger isolation pressure testHighly accurate for detecting invisible leaks between the combustion zone and the air streamRequires much more time to properly seal off the exchanger and set up the measurement toolManometer, temporary sealing materials

While a flame displacement test (watching if the flame wavers or dances when the blower motor kicks on) is a great initial check, it is not enough to officially condemn a furnace. A combination of a combustion gas analyzer to read ambient and flue CO levels, followed by a thorough visual inspection using a borescope, is the industry best practice.

Should I replace the heat exchanger or the entire furnace?

Once you have verified that the furnace heat exchanger is cracked, the next step is advising your customers. You cannot safely weld, seal, or patch a cracked heat exchanger. The only safe and legally compliant options are replacing the heat exchanger itself or replacing the entire furnace.

The decision between replacing a heat exchanger in furnace vs. installing a brand new unit often depends on the age of the system, warranty coverage, and the overall condition of the remaining components.

When to choose heat exchanger replacement

Replacing just the heat exchanger might be the right call in specific situations. Consider recommending a part replacement in the following job scenarios:

  • The furnace is under warranty: If the system is relatively new, typically under 10 years old, and the manufacturer's warranty covers the cost of the replacement part, this is usually the most cost-effective route for the customer.
  • The rest of the system is pristine: If the blower motor, control board, and inducer are testing perfectly and show no signs of excessive wear, swapping the heat exchanger can add years of life to the furnace.
  • Strict budget constraints: If the customer absolutely cannot afford a full system replacement and the exact part is available quickly, replacing the exchanger provides a safe, albeit temporary, solution.

However, always remind customers that they will still be responsible for the labor costs, which can be substantial given the time required to tear down the furnace and rebuild it.

When to choose a full furnace replacement

In many cases, investing in a brand-new system is the wiser financial decision for the homeowner. You should recommend a complete furnace replacement when:

  • The furnace is old and out of warranty: If the unit is over 12 to 15 years old, the cost of the replacement part — plus labor — is too high to justify a system nearing the end of its life expectancy.
  • Multiple components are failing: If you notice a failing inducer motor, rust on the burners, or a weak capacitor during your inspection, replacing just the heat exchanger is a bad investment.
  • The original system was oversized: If an oversized furnace is what caused a heat exchanger to crack in the first place, putting a new exchanger into an improperly sized unit will just lead to the same failure down the road. Upgrading allows you to properly size a new unit for their ductwork.
  • The customer wants better efficiency: Older furnaces with cracked exchangers are often standard efficiency (80% AFUE). Upgrading to a high-efficiency condensing furnace (90%+ AFUE) will provide long-term energy savings.

Discussing how much routine HVAC service lowers bills in the long run can help customers see the value in a new, highly efficient system over a costly repair to a deteriorating unit.

Partner with Ferguson

Furnace heat exchanger diagnostics demand precision and a strict commitment to safety. By understanding the root causes, recognizing the symptoms early, and utilizing a combination of combustion analysis and visual inspection, you can protect your customers from the silent dangers of carbon monoxide.

When a crack is verified, guiding homeowners through the complex decision of replacing the heat exchanger vs. installing a new furnace requires honesty and a clear explanation of the long-term costs. Complete the job with confidence by shopping Ferguson's extensive inventory of heat exchangers or speaking with one of our knowledgeable associates today.